From Shrimp To Scrap | Cummins Inc.
""
Marine

From Shrimp To Scrap

by Alan Haig-Brown

Cummins Vessel Reference #576

Photo courtesy of B&J Martin, Inc

“We are still working on three platforms that were damaged by Katrina in 2005,” says Jimmie Martin of Galliano Louisiana. Martin’s firm, B&J Martin Inc., operates crew and supply boats in the Gulf of Mexico, but their signature work is their site clearance operation.

The US Mineral Management Services (MMS) mandated in 1990 that all abandoned well sites and platforms had to be cleaned in such a way that a commercial shrimp trawler could work the bottom without damaging their nets. This and subsequent regulatory modifications has created a demand for the vessels, gear and services that B&J Martin provides. The regulations require that the contracted owner “must possess a valid commercial trawling license” from one of the Gulf States. Since the Martin family has a long history of Gulf shrimping this is a natural. For site verification (i.e. that it has been cleaned), “The trawling vessel must be outfitted with trawling nets that are representative of the accepted shrimping industry standard of up to No. 18 twine (ribbon strength) size net strength.”

The regulations give very specific details that relate to the verification that the site is clean. But to get it clean, to catch all the stuff that has fallen or been blown over board, requires a different set of nets. To this end Martin’s company has patented the Gorilla Net. This gear employs a weave of 3/4-inch combination cable at its opening with a body made of twine five-times the strength of a standard trawl net.

Martin’s boats tow two 80-foot Gorilla nets in the clean-up phase of the operation. “If we are lifting all tires we can bring up five or six tons per net,” explained Martin, “But if it is square stuff or has sharp edges we are more limited. On one well we brought up a total of 200 tons of scrap.”

Martin has grown his fleet to include two 85-footer single-screw boats, one 95-foot single screw and a 100-foot twin-screw boat. Recently they had a powerful 110 by 28-foot shrimper style vessel built at Rodriguez Shipyard in Bayou La Batre. Rodriguez has built a lot of shrimp boats in the past but this new boat shares a bit of heft with the jack-up boats that Rodriguez has been building of late. The new shrimper/clean-up boat is built much heavier than a conventional Gulf shrimper. Named the Poncho, it is powered by a pair of 850-HP Cummins KTA38 main engines turning into Twin Disc 5321 gears with 6:1 ratios. This adds up to 1700 HP that is a good bit more power than a conventional shrimper, but it is power that will be put to good use scraping pieces of oilrig off the bottom of the Gulf of Mexico. The new boat from Rodriguez is also fitted with two Cummins-powered 65 kW generator sets.

There is plenty of work for the new boat. Martin explains that to tow the grid on a 1320-foot radius around a platform will take about 4.5 days when it is all cleaned up. But they have spent up to 90 days cleaning the mess created when hurricane Katrina tipped a rig into the Gulf.

The final part of a clean up requires that conventional gear be towed over the area, Martin uses four 50-foot nets with two-inch mesh. This is equal to what most shrimpers in the area are using. For the clean up to be approved these lighter nets must be towed on a north-south and then an east-west grid. The trawl tracks are recorded utilizing a GPS plotter to demonstrate that the bottom is once again suitable for shrimping.

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...