Truck driving on highway away from sun setting
Experience the future of power on the Forever Rising Tour

See how Cummins’ latest engines - including the 2027 X15, X15N, and X10 - perform in real‑world, ride‑and‑drive environments. Discover the technology shaping the road ahead.

Learn about tomorrow - today

x15 next gen engine
Featured Heavy-duty truck engine

The 2027 X15

Introducing the 2027 X15 engine. The next step in the Cummins HELM™ 15-liter platform. Offering up to 605 hp and 2,050 lb-ft torque, this engine demonstrates our continued commitment to the evolution of internal combustion technology.

Click here for more information
x10 engine
Featured Heavy-duty truck engine

X10

Introducing the new Cummins X10, a next generation engine that brings a state-of-the-art platform to medium-duty, heavy-duty, vocational, and transit bus applications, launching in North America in 2026. This engine is uniquely positioned to replace both the L9 and X12.

Click here for more information

Choosing the right heavy-duty truck engine

Cummins diesel engines are favorites in the North American heavy-duty truck market. Drivers, owner/operators, and fleet managers agree: Cummins engines are among the most powerful and reliable Class 8 truck engines on the road.

 

Heavy-duty truck engines by use case and primary benefit

Use case Primary benefit Engine recommended 
Long hauls Efficiency X15 Efficiency Series
Multi-purpose Continual access to peak horsepower X15 Productivity Series
Premium linehaul More than 500 HP X15 Performance Series
Weight-sensitive vocational or regional haul Maximum payload X10 Engine

Heavy-duty truck fleet optimization tools

Make confident decisions faster with tools that simplify your journey

Power Selection Tool

Find the ideal power solution for your truck fleet by completing a short survey to evaluate your best-fit power type.

Product Availability Tool

Find the right heavy-duty truck engine and transmission combination for your vehicle application.

PowerSpec

Build your next heavy-duty truck with precision - guiding you through the process of spec-ing a Cummins-powered vehicle.
woman standing in front of fleet of heavy duty trucks
Remotely manage your fleet

See how to proactively monitor your heavy-duty truck fleet to help maximize driver safety, vehicle uptime, and operational efficiency.

Frequently asked questions

Heavy-duty truck engines are usually diesel or natural gas engines designed for Class 8 semi-trucks used in demanding commercial applications. These engines are built to deliver high horsepower to meet needs such as maximum payload capacity, long-haul efficiency, and continual access to peak power. These powerful engines are engineered for use cases ranging from weight-sensitive vocational and regional haul work to multi-purpose, long-distance commercial trucking.

The best heavy-duty truck engine is subjective and highly depends on your use case. We recommend the following based on the intended use:

To choose the right heavy-duty truck engine, please consider the needs for your use case:

The following fuel types are available for heavy-duty truck engines:

  • Diesel: A relatively cheap fuel that’s widely available and performs well with durable and reliable engines that provide all the torque needed for heavy-duty applications.
  • Renewable Diesel (HVO): A fuel made from vegetable oils and animal fats. It can often be used as a drop-in replacement for diesel with no engine modification with net CO2 emissions typically 70% lower than diesel.
  • Biodiesel: A renewable fuel most often blended with diesel. B20 blends balance cost and emissions and can generally be used with no engine modifications (always check with the manufacturer and truck manual before using).
  • Natural Gas (CNG/LNG): A fuel that can be used in either compressed or liquefied form. Natural gas performs similarly to diesel with lower CO2 and reduced NOx and particulate emissions.
  • Renewable Natural Gas (RNG): A fuel produced from biogas captured from organic waste. RNG can help fleets reach sub-zero greenhouse gas emission levels.
  • Hydrogen: Cummins is developing hydrogen internal combustion engines, including a 15-liter and 6.7-liter version for heavy-duty commercial applications.
  • Battery Electric: Battery electric trucks significantly reduce operating costs due to lower fuel and maintenance expenses. With zero tailpipe emissions, they contribute to cleaner air quality and the reduction of greenhouse gas emissions. Cummins offers battery electric solutions through Accelera™ by Cummins.

Cummins heavy-duty truck engines include the X15 Efficiency Series, X15 Productivity Series, X15 Performance Series, X12, X15N, the 2027 X15, and the new X10.

""
The future of energy transition

Transportation has evolved since the beginning of time. What does the future of transportation hold?

Going further, faster

highway alongside forest and lake
Destination Zero

It’s our mission to power a more prosperous world.

We do this by helping customers succeed through innovative and dependable products that are good for our customers and the environment.

Heavy-duty truck engine parts and service

Service to keep you moving

Choose from our network of over 9,000 service and distributor locations around the globe.

Extend the life of your engine with Genuine Cummins Parts

There is a difference. There’s no match for Genuine Cummins Parts.
Connect with us