Norfolk Tug and Lyons Shipyard Continue Upgrades | Cummins Inc.
""
Marine

Norfolk Tug and Lyons Shipyard Continue Upgrades

by Alan Haig-Brown

Cummins Vessel Reference #732

The Captain D: all dressed up and ready to go.

Established in 1928 by George Lyon Sr, Lyon Shipyard today occupies 30 acres of waterfront near downtown Norfolk Virginia. Norfolk Tug is based in the same area and takes pride in operating a fleet of tugs from the 1970s and ‘80s that they proudly designate as “vintage steel”. They also have an aggressive program of updating these beauties with extensive upgrades, including new engines, generators, wiring, shaft seals as well as piping and wiring renewal wherever necessary.

One of their vessels, the 92 X 26 X 11 Captain D, was taken into Lyons Shipyard for an extensive rebuild in 2008. At that time they repowered a number of tugs with Tier 2 compliant engines. Now, only six years later, they have again sent the Captain D over to Lyons. This time she has been upgraded with Tier 3 complaint Cummins engines. The Tier 2 Cat 3508C engines were pulled and replaced with Tier 3 compliant QSK38-M engines.

Originally built and launched from Bollinger Shipyard in 1974, the Captain D, is entering its fifth decade of life with her original quality steel work and state of the art machinery. The updated tug also has an Intercom towing winch with 1.5-inch wire and, for pushing, a set of stern chocks with Spectra push gear. Back in service again, the Captain D promises many more years of reliable service.


For further information:

Richard Sutton
Marine Territory Manager
Cummins Power Systems LLC
106 Wells Cove Rd.
Grasonville, Md. 21638
Phone: 410 690 3612
Mobile: 443 690 2986
Fax: 410 590 8731
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...