Case Studies | Cummins Inc.

Cummins Case Studies

We’re in it for the long haul. We build lasting partnerships that lead to smarter innovations for our customers. These customer stories demonstrate our commitment and success in providing customers like you with improved power solutions through world-class innovation in a number of industries.

Filter Case Studies

Purpose: To develop and ensure the efficient operation of multiple hyperscale data centers, enhancing Saudi Arabia’s digital infrastructure.

Kyle Myrick is a proud owner of a 2015 Cummins Turbo Diesel-powered Ram Tradesman pickup truck, with over 300,000 miles on the odometer. As a mining engineer with over 20 years of experience, his truck is continuously put to the test in harsh environments—not only as part of Kyle’s work but also in support of his passion for travel and adventure.

Purpose: Upgrade a 20-year-old legacy DMC to enhance the power system capacity and reliability for a major network and communication service provider in Saudi Arabia.

STAMFORD P7 alternators play a critical role in powering the Ambatovy Project, a landmark mining and processing development in Madagascar.

Cloud boom behind Naver’s  supremacy push With soaring traffic on its platform, Naver embarked on the project to construct one of Asia’s largest data centers which will be developed over six phases using a substantial volume of generator sets.  The first phase of the Gak Sejong data center features 18 Cummins QSK95 gensets with a 60 Hz standby rating of 37

Ensuring uninterrupted healthcare services, Arken Generator’s advanced synchronization system provides Sivas Cumhuriyet University Hospital with reliable, continuous power. Discover how innovative power solutions enhance patient safety, operational efficiency, and sustainability goals. Reliable power solutions from Arken Generator Founded in 2012, Arken Generator operates from its state-of

Elcos, in partnership with STAMFORD | AvK, delivers a robust standby power solution for a pharmaceutical manufacturer in Switzerland. Discover how proven reliability supports continuous operations in the highly regulated pharmaceutical industry. Ensuring continuous power for critical pharmaceutical production Elcos is one of Italy’s leading power generation companies, with over 45 years of

Genmac, in partnership with STAMFORD | AvK, delivers dependable standby power to support the critical signalling system at a Paris train station substation. Learn how robust generator solutions ensure continuous operation for the National French Railway Company. Ensuring seamless operation of train traffic signaling systems in France With over 40 years in the generator manufacturing indust

Green Power Systems delivers essential backup power solutions for healthcare, ensuring hospitals like those in England maintain uninterrupted operations. Discover how our specialized technology supports critical patient care during power outages. Specialized power solutions for healthcare: reliable, efficient, and tailored for critical operations Green Power Systems Srl, a leading Italian

Arken Generator, in collaboration with STAMFORD | AvK, powers critical operations at Turkey’s Ermaden Coal Mine.

Project background The upgrade was necessary as the legacy DMC300 reached end-of-life due to obsolete hardware components and software. Additionally, the customer aimed to add more generators and required changes in the control sequence to enable integration with a PV renewable system. Challenges The legacy DMC300 was equipped with outdated PLCs, having obsolete software and hardware modu

Overview Where: Johannesburg, South Africa Purpose: To reduce carbon emissions and take a significant step towards Cummins 2030 Environmental Social and Governance (ESG) goals Supply: PowerCommand Microgrid Control® MGC900, 700 AC kWp of Solar power, Two KTA 38G5 Diesel Generators     Cummins South Africa installs Microgrid System in Power Hub Headquarters Cummins is act

Expanding Cummins footprint at Maules Creek Whitehaven Coal, noted for producing high quality thermal and metallurgical coal, has four operating mines in the Gunnedah Basin which achieved run-of-mine (ROM) production of 18.2 Mt in 2023. More than 100 high horsepower Cummins engines are involved in its three open-cut operations, including the Maules Creek operation which is repowering five Hitac

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern shore of the Greek mainland, passengers feel the wind in their hair and magic in the air approaching the world’s most incredible, secluded beaches nestled away on remote islands accessible only by boat. Boasting 10,000 miles of coastlines

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea Rae, whose fish tale about five-year-old angler prodigy, Wyatt Goodwin, catching the big ones, is true. Wyatt’s ride is a new 37-foot APB Custom Blackfin, recertified by the Coast Guard as a new build in 2022. Wyatt’s father, Nate Goodwin,

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fishing boats. Characterized by a bow with high guard rails to protect the owner and crew on deck, trawlers are built with long-range cruising ability at an average speed under 10 knots. The deck’s clutter-free design enables seawater po

High speed ferry powered by Cummins QSK95 engines Tanzania’s latest fast ferry joins a fleet of vessels numerically named after the country’s majestic, dormant volcano. Built for Azam Marine, Kilimanjaro VIII is a 53m aluminum, passenger fast ferry cruising between Dar es Salaam and the historic spice island of Zanzibar. With a top speed of 37 knots at 8,000 horsepower, the vessel transits 620