Cummins Power for Incat Crowther Crewboat | Cummins Inc.
""
Marine

Cummins Power for Incat Crowther Crewboat

by Alan Haig-Brown

Cummins Vessel Reference #698

The Swissco Cheetah delivered from Cheoy Lee's Zuhai shipyard photo courtesy of Cheoy Lee Shipyard.

Hong Kong Based Cheoy Lee Shipyard recently delivered the first of two 36 by 7.6-meter crew boats from their shipyard in Zuhai China. Designed by Incat Crowther the Swissco Cheetah’s red mono-hull has capacity for 50 tons of cargo on its 94 square meter after deck. Built to ABS class the vessel’s tankage includes 57,400 liters of fuel and 21,250 liters of fresh water. Accommodation is provided for ten crewmembers in six cabins and seating for up to 70 passengers. Forward doors in the deck cabin permit the option of transferring personnel from the bow.


A distinctive Incat Crowther design photo courtesy of Cheoy Lee Shipyard.

The Cummins Hong Kong branch supplied the three Cummins KTA38-M3 HD engines that power the Swissco Cheetah. Each engine delivers 1007 kW (1350 bhp) at 1900 RPM to fixed-pitch propellers through Twin Disc reduction gears. This gives the vessel a 24-knot service speed and a top speed of 27 knots.

Incat Crowther information points out that, while this is the first of this design built by Cheoy Lee, there is a continuing strong relationship between the designer and builders. A sister-vessel will deliver later this year. At the end of May the Swissco Cheetah is based in Singapore preparing for its first assignment. Cummins Sales and Service Singapore Pte Ltd will provide after-market support.


For further information:

Sean Lynas
Director – Regional Engine Sales (NE/SE Asia)
Cummins Singapore
8 Tanjong Penjuru
Singapore
Phone: 65 6661 8283
Mobile: 65 9 66 55 851
E-mail: [email protected]

Yin Nin Mou
Branch Manager
Cummins Hong Kong
Lok Tung Street, On Lok Tsuen,
Fanling, Hong Kong
Telephone: 852 2606 5678
Fax: 852 2687 3552
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...