Indian Built for Indian Firm | Cummins Inc.
""
Marine

Indian Built for Indian Firm

by Alan Haig-Brown

Cummins Vessel Reference #710

The Orion Laxmi

Goa, India’s Mandovi Drydocks has made significant contributions to the domestic boat building industry. A good example of this is the 43 by 10-meter off shore supply vessel M.V. Orion Laxmi owned by Orion Off Shore Services Pvt. Ltd.


Stern view of the Orion Laxmi

Delivered to her owners at the end of 2011 the vessel has a clear deck space of 183 square meters and a total deck area of 220 sq.m. Main engines are a pair of Cummins KTA 38-M2 each producing 1200 HP at 1800 RPM. This provides a 20-ton bollard pull for towing with a towing hook. The vessel is fitted with an ‘A’ frame and a three-ton capstan. Tankage includes 84 tons of fresh water and 386 tons of diesel oil.


Photos courtesy of Mandovi Drydocks


For further information:

Girish Uttamchandani
Business Leader – Shipyard
Cummins India Ltd.
E-mail: [email protected]
Phone: 91 20 3023 3716 | Extension: 3716
Mobile: 9922956359

Kanekar Rajesh
Mandovi Drydocks
Pigao, Goa, India
E-mail: [email protected]
Phone: 9822130448

Orion Offshore Services Pvt. Ltd.
“A” Wing, Dhanashree,
Dilip Gupte Road,
Near Hinduja Hospital,
Mahim (West),
Mumbai 400 016
India
Phone: 91 022 1445 8665 | 91 022 6507 2396
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...