Norwegian Diesel Electric Joins Trend | Cummins Inc.
""
Marine

Norwegian Diesel Electric Joins Trend

by Alan Haig-Brown

Cummins Vessel Reference #582

The Stril Mariner on seatrials - Cummins photo.

The world’s leading offshore shipping companies are increasingly turning to diesel electric propulsion systems as an efficient means of meeting the performance requirements for modern platform supply vessels. Builders in the US, China, Singapore and Norway have all delivered a variety of diesel electric vessels.

In Norway the shipyard of Simek A/S has been a leader in the technology. Recently they followed up earlier vessels when they delivered the M/S Stril Mariner to Simon Møkster Rederi AS in Stavanger, Norway. The Stril Mariner, named at a ceremony on October 30, 2009, is 78.6 meters long with a 17.6-meter beam and a moulded depth to the main deck of 7.7 meters. With a 3755 deadweight tonnage the PSV has tankage for: 910 cubic meters of fuel oil, 925 m3 of fresh water, 1250 m3 drill water and 1010 m3 each of mud, liquid mud and brine. Additional tankage includes 175 m3 of methanol, 150 m3 of glycol, 315 m3 of dry cargo and 1300 m3 for ORO. The cargo deck is 755 square meters.

Accommodation is provided for 31 people in 11 one-man cabins and 10 two-man cabins. There is also a deck office, a hospital and a conference room. The vessel is certified by ISO 9001:2000 (Quality) and ISO 1401:2004 (Environmental). Designed by the Havyard firm of naval architects (www.havyard.com) the Stril Mariner has all tankage installed so that there is no storage of liquids that could harm the environment against the ship’s hull shell.

In addition to this and other provision, the vessel gains its “green” designation as a result of the diesel electric propulsion system. As only the engines required to maintain the task as hand need be running the resulting emissions, as well as fuel costs, can be dramatically reduced. To achieve this flexibility in the main propulsion system the Stril Mariner is fitted with four Cummins KTA50-(D)M engines each of which turns a generator to produce up to 5,164 kW of power. This can drive the two azimuthing (Roll-Royce Marine AS, Ulstein Aquamaster, model US 205 CRP ) drives for main propulsion as well as a pair of bow thrusters. Engines and generators can be shut down when holding position or travelling at reduced speed thus reducing the released pollutants. Additionally the main engine exhausts have been fitted with a Selective Catalytic Reduction (SCR) exhaust gas cleaning system, cleaning the environmentally hazardous CO (carbon monoxide), NOX (nitrogen oxides) and VOC (hydrocarbons) in the exhaust with ammonia, and the nitrogen oxides of the exhaust gas becomes environmentally natural substances water (H2O) and Nitrogen (N2), thus reducing the NOX by approximately 90%.

As diesel electric and other initiatives to contain operation costs while reducing a ship’s environmental impact proliferate the vessels become ever more complex. In that context the classification societies have a greater challenge. It is no longer just about hull plating welds and shaft alignment. The Stril Mariner is classed by DNV with Class Notation * 1A1 Fire Fighter I OILREC SF LFL* COMF-V(3) E0 DYNPOS-AUTR NAUT-OSV(A)CLEAN DK(+) HL(2.8).

A sister ship to the Stril Mariner is slated for delivery in the spring of 2010.

For further information:

Sjoerd Spronck
Advertisement & Promotion
Scandinavia and Benelux
Cummins Holland B.V.
Olivijn 800
3316 KH Dordrecht
The Netherlands
Tel; 31 78 6530 927
Fax: 31 78 6176 579
E-mail: [email protected]
Web: www.cummins.com | www.cummins.nl

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...