Triple Z-Drive Pushboat | Cummins Inc.
""
Marine

Triple Z-Drive Pushboat

by Alan Haig-Brown

Cummins Vessel Reference #752

Pushing up the Ohio River at Padukah Kentucky. (Jeff L. Yates photo)

Long talked about and occasionally experimented with, the Z-drive is rapidly gaining acceptance on America’s inland waterways. While a number of operators have recently built boats powered by a pair of Cummins 1000 HP K38 M engines and Z-drives, Main Ironworks is building a series of four boats with three Cummins 750 HP QSK19-M engines coupled to well-mount ZF WM5000 drives. This combination gives the boats a similar, but slightly higher, 2250 HP with greater flexibility for rebuild and maintenance of EPA tier requirements. The engines are set on the main deck level of the 11-foot molded depth hull, to give the boat an operating draft of ten feet which includes the one-foot plate keel that helps protect the Z-drives in conjunction with the stump jumpers.

Four of the 79.5 by 34-foot boats, Jock Cenac, Eugenie Cenac, Jack G. Cenac, and Loretta G Cenac have been delivered. Acceptance of new approaches can be slow on the inland waterways, but the Z-drive is rapidly gaining prominence as a means of propulsion in the 2000-HP class of pushboat.


For further information:


Marc Molaison
General Manager
Main Iron Works Shipyard
148 Old Ferry Rd.
Houma, LA 70364
Phone: 985 876 6302
E-mail: [email protected]

Mike Lee
Territory Sales Manager
Cummins Mid-South Inc.
Kenner, LA
Phone: 504 734 3075
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...