Twelve Good Boats | Cummins Inc.
""
Marine

Twelve Good Boats

by Alan Haig-Brown

Cummins Vessel Reference #599

The Pass Christian at the Smithland Lock. photo by Jeff L. Yates

 

Already the operator of the largest fleet of inland tank barges on US inland waters, Kirby Marine Transportation, has recently added twelve more push boats to its fleet. The twelfth in a series of sister vessels was delivered from Raymond and Associates of Bayou LaBatre, Alabama in late July 2010.

 

All twelve of the 1700 HP boats are 76 by 35-feet in length. Each boat is powered by a pair of Tier 2 compliant Cummins K38-M diesels rated for 850 HP each at 1800 RPM. The engines turn big 76 by 56-inch five-blade props through Twin Disc TD MT540 gears with relatively large ratios of 7:1.

The most recently delivered towboat was the M/V Ellis Davis. An earlier vessel in the series is the M/V Pass Christian that was delivered in September of 2009. The attached photo of the Pass Christian was taken by Jeff L. Yates this August 17 on the Ohio River as the boat locked up at Smithland Lock. The locks are located 62 miles up from the confluence of the Ohio and Mississippi Rivers and 918 miles below Pittsburgh, Pennsylvania.

 

For further information:

 

Jay Rowan
Cummins Southern Plains, Inc.
7045 N. Loop 610 East
Houston, Texas 77028
USA
Phone: 713 679 2220
E-mail: [email protected]
Web: www.cummins.com/sales-and-service

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...