World’s Leading Manufactures for Russian Tug | Cummins Inc.
""
Marine

World’s Leading Manufactures for Russian Tug

by Alan Haig-Brown

Cummins Vessel Reference #791

The Grifon-8 ready for work.

Russia’s Pella Shipyard advertises a range of five ASD tugs. Their model 90600 has proven popular with satisfied customers returning for sister ships. Currently the yards has one of these handy-sized 25.4 by 8.8-meter tugs under construction for the Grifon Company.


The profile and GA of a Pella docking tug.

With a long list of design features, including fi-fi capabilities, centralized controls in the wheelhouse, and operational reliability in severe ice conditions. This latter provision is enhanced by the below water hull design at the stern to protect the Z-drives from ice damage while the bow is designed for ice breaking. The double chine hull and slightly extended keel for and aft provide directional stability while not limiting maneuverability.

A pair of Pella tugs at work.

The builder’s prospectus promises “installation of equipment of the world’s leading manufacturers. For propulsion a pair of Cummins K50-M diesels meets this standard with each delivering 1193 kW (1600 HP) at 1800 RPM in a continuous duty rating. The engines drive Rolls Royce Z-drives giving the tug a free running speed of 12 knots and a bollard pull between 23 and 35 tons depending on owner’s specifications.

Two Cummins 6B-CP80DMS-powered gen sets each provide 80 kW of electrical power for ship’s use including the electro-hydraulic anchor winch and deck crane. Accommodation is provided for eight crewmembers while tankage includes; fuel oil 70 m3, lube oil 1.6 m3, fresh water 12 m3, ballast 18 m3.

The tug is being built to the Russian Maritime Register of Shipping class KM Ice2-Arc4 R3 AUT3 FF3 WS Tug.


Photo and GA courtesy of Pella Shipyard

For further information:


Marketing Department
Pella Shipyard
4, Tsentralnaya str., Otradnoye,
Kirovsky district, Leningrad region,
187330 Russia
Tel/fax: 7 812 336 4067
E-mail: [email protected]
Web: http://www.pellaship.ru/en/

Alexander Dunkov
Marine Sales Manager
Cummins Russia and CIS
Phone: 7 812 57007798
Mobile: 7 961 800 06 42
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...