Xin Yue Feng: Growth with a Range of Vessels | Cummins Inc.
""
Marine

Xin Yue Feng: Growth with a Range of Vessels

by Alan Haig-Brown

Cummins Vessel Reference #762

 

 

The Cummins Swissco Garnet powered by a pair of Cummins KTA50-M2 mains producing a total of 3200 HP.

 

From the four-story office tower, housing 100 technical engineers and administration staff, to the 65,000-square-meter yard with extensive fabrication and machine shops and a huge dry dock, the Xin Yue Feng Shipyard has been building every more sophisticated vessels. Although the majority of the yard’s work is in steel, they maintain a set of skilled aluminum workers as well. In mid-March this group was building a small aluminum service vessel for a Singapore customer. Over in the yard’s assembly and launch dock, four big DP2 anchor handlers were in various stages from fabrication with the aide of an overhead gantry crane. Nearby another AHT was being finished at the fitting out dock.

 

 

Xin Yue Feng Shipyard’s Chairman Luo Chaoneng with a pair of AHTs under construction.

 

Also in the water, and awaiting delivery by ship to Jeddah, Saudi Arabia, were two 15-meter and one 12-meter line handling or mooring boats. Each of these is powered by a pair of Cummins NT855 each delivering 261 kW at 1800 RPM. Back in the office block the walls are lined with photos of recently delivered vessels. Shipyard Chairman Mr. Luo Chaoneng points out the 39.8 by 10.5-meter BADR 5, delivered this year to a Saudi Arabian customer. A pair of Cummins QSK19-M engines each producing 597 kW at 1800-RPM powers this handy-sized tug.
 

 

The yard has delivered a number of smaller aluminum vessels and has plans for a 40-meter crew boat.

 

Nearby sporting a hefty knuckle-boom is a picture of the 34 by 10-meter anchor handling tugs Swissco Garnet. Delivered this past January, the AHT has a molded depth of4.7 meters. Classed by BV it received the notation [1 +HULL +MACH, tug, Special service – Anchor Handling, Unrestricted Navigation]. Powered by a pair of Cummins KTA50-M2 mains producing a total of 3200 HP to give the boat a 40-ton bollard pull and 11-knot speed. The Swissco Garnet is a repeat order and sister ship to the Swissco Opal delivered in 2013.

 

 

The Bader 5 is powered by a pair of Cummins QSK19-M shortly before leaving the yard for her Saudi owners.

 

As a privately owned shipyard since 2006, the Xin Yue Feng Shipyard exhibits a professionalism and dedication to quality that is earning repeat orders from some of the worlds leading off-shore companies.

 

 

Three mooring boats built to BV class with two Cummins NT855 mains.

 

Photos courtesy of Xin Yue Feng Shpyard except #2&3 by Haig-Brown.

 

For more information:

 

Mr. Luo Chaoneng
Chairman
Xin Yue Feng Shipyard Ltd.
Jinmen Industrial Park,
Sadui Town, Xinhui District
Jiangmen City,
China, 529147
Phone: 86 750 623 2780
Mobile: 86 1380 283 4728
E-mail: [email protected]

Enrique Yip
General Manager Assistant
Xin Yue Feng Shipyard Ltd.
Phone: 86 750 623 3902
Mobile: 86 139 288 1828
E-mail: [email protected]

Linda Zhang
Manager: Southern China
Cummins Inc., East Asia Marine
Phone: 86 20 3998 2999
Mobile: 86 136 0004 0695
E-mail: [email protected]

Weney Lee ???
Customer Support
Cummins Dealer
Yinpeng Group
No.5, Yihengxi Road,
Dongsha, Panyu,
Guangzhou,
Guangdong China
Phone: 86 20 84872872
Mobile: 1371 940 5000
URL: www.yinpeng.com
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...