Diesel Generators | Cummins Inc.

Diesel Generators

generator assembly plant

Choose from a wide array of CPCBII compliant diesel generator specifications

High fuel efficiency generators, low emission levels, 24x7 service support

Cummins understands how essential uninterrupted power is for all – home, business and commercial. Powered by the technologically advanced power generation solutions starting from 7.5 kVA to 3750 kVA, our product range is geared to take on the most challenging applications.

Our power solutions are built to deliver consistent performance across all industry segments, ensuring that you always stay ahead of the rest. We promise quality products and exceptional customer support.

 

Browse our products below or use one of the links to contact us for more information

Service Network      Send Enquiry 

 

Availability: The products listed in this page are for sale in the Indian subcontinent only.

Key Generator Set Specifications:

 

7.5 - 15 kVA
Genset Model kVA (Prime) Engine Model BHP Alternator Frame Genset Controller Brochure
C7.5D5P 7.5 X1.3TAA-G1 23 PI044D (3Ph) / PT044F (1Ph) PSO600
C10D5P 10 X1.3TAA-G1 23 PI044E (3Ph) / PT044G (1Ph) PSO600 Download the brochure for 7.5-15kVA
C15D5P 15 X1.3TAA-G1 23 PT044G (3Ph) / PT144D (1Ph) PSO600
20 - 30 kVA
Genset Model kVA (Prime) Engine Model BHP Alternator Frame Genset Controller Brochure
C18.5D5P 18.5 X1.3TAA-G7 25.2 S0L2-U1 PSO600 Download the brochure for 18.5kVA (1Ph)
C20D5P     20 X1.3TAA-G7 25.2 S0L2-M1 PSO600 Download the brochure for 20kVA (3Ph)
C30D5P 30 X2.7TAA-G2 38.5 S0L2-P1 PSO600 Download the brochure for 25-30kVA
35 - 40 kVA
Genset Model kVA (Prime) Engine Model BHP Alternator Frame Genset Controller Brochure
C35D5P 35 X2.7TAA-G7 47.5 S1L2J1 PSO600 Download brochure for 35-40kVA
C40D5P 40 X2.7TAA-G8 51 S1L2K1 PSO600
50 - 62.5 kVA
Genset Model kVA (Prime) Engine Model BHP Alternator Frame Genset Controller Brochure
C50D5P 50 4BTAA3.3-G11 84 S2L1D-D4 (3ph) UCI224G( 1Ph) PSO600 Download the brochure for 50-62.5kVA
C62.5D5P 62.5 4BTAA3.3G11 84 S2L1D-E4(3Ph) UCI274D(1Ph) PSO600

82.5kVA
Genset Model kVA (Prime) Engine Model BHP Alternator Frame Genset Controller Brochure
C82.5D5P 82.5 4BTAA3.9-G4 110 UCI224G PSO600 Download the brochure for 82.5kVA
100 - 125 kVA
Genset Model kVA (Prime) Engine Model BHP Alternator Frame Genset Controller Brochure
C100D5P 100 6BTAA5.9-G13 159 S3L1D-C41 PSO600 Download the brochure for 100-125kVA
C125D5P 125 6BTAA5.9-G13 159 S3L1D-D41 PSO600
140 -160 kVA
Genset Model kVA (Prime) Engine Model BHP Alternator Frame Genset Controller Brochure
C140D5P 140 QSB5.9-G1 184 UCI274E PC 1.1 Download the brochure for140-160kVA
C160D5P 160 QSB5.9-G2 206 UCI274F PC 1.1

Genset Model kVA (Prime) Engine Model BHP Alternator Frame Genset Controller Brochure
C180D5P 180 QSB6.7-G14 234 UCI274G PC1.1 Download the brochure for 180-225kVA
C200D5P 200 QSB6.7-G15 256 UCI274H PC1.1
C225D5P 225 QSB6.7-G16 280 UCI274K PC1.1
C250D5PE 250

QSB6.7-G17

307 UCI274G PC1.1 Download the brochure for QSB6.7 - 250kVA 
C250D5P 250 6L8.9TAA-G4 335 UCI274K PCO600 Download the brochure for L8.9 - 250kVA
C275D5P 275 QSL9-G16 334 HCI444D PC1.1 Download the brochure for 275-320kVA
C300D5P 300 QSL9-G15 399 HCI444D PC1.1
C320D5P 320 QSL9-G15 399 HCI444D PC1.1
C400D5P 400 QSN14-G2 486.5 HCI444F PC1.2 Download brochure for 400kVA
C500D5P 500 KTAA19-G10 587 HCI544D PSO601 Download the brochure for 500kVA

Genset Model kVA (Prime)  Engine Model BHP Alternator Frame Genset Controller Brochure
C600D5P 600 KTAA19-G12 713  HCI444E   PC3.3 Download the brochure for 600kVA

Download the brochure for 625kVA

Download the brochure for 650kVA

C625D5P 625 KTAA19-G13 739 HCI444E PC3.3
C650D5P 650 QSK19-G7 828.5 HCI544F PC1.2
C750D5P 750 KTA38-G12 1069 HCI634W PC3.3 Download the brochure for 750-810kVA
C810D5P 810 KTA38-G12 1069 HCI634V PC3.3
C910D5P 910 KTA38-G17 1069 HCI634Y PC3.3 Download the brochure for 910kVA 

 

 

Genset Model kVA (Prime) Engine Model BHP Alternator Frame Genset Controller Brochure
C1010D5P 1010 KTA38-G5 1180 HC6Y PC3.3 Download the brochure for 1010kVA
C1250D5P 1250 KTA50-G3 1470 HCK6Z PC3.3 Download the brochure for 1250-1500kVA
C1500D5P 1500 KTA50-G8-I 1735 PI734C PC3.3
C1800D5P 1800 KTA50-G22 2101 S7L1D-G4 PC3.3 Download the brochure for 1800kVA
C2000D5P  2000 KTA50-G21 2334 S7L1D-G4 PC3.3 Download the brochure for 2000kVA 

Frequently Asked Questions

Based on applications, diesel generators include portable generators, inverter generators, and standby generators. Portable or small generators can easily be placed and is used mainly in local area shops like hotels, stores, car, and bike showrooms to different appliances. Inverter generators produce more AC electrical energy per engine rotation so the raw electricity transforms into DC power. Both of these generators can power various types of tools and appliances depending on the item’s running and surge wattage. A standby generator operates automatically by sensing power cuts. They are used for backups as industrial, residential, or commercial diesel generator.

There are many eCommerce aggregator stores and websites where diesel generator options are available for sale. If you want to purchase one directly from a diesel generator company, companies like Cummins have many options available. You can get detailed product brochures, choose your specification and diesel generator price, and send in an enquiry for purchase. You can also place bulk orders for different generators. You can use one of the links below to contact us for more information:

Service Network      Send Enquiry 

Kilowatt (or 1000 watts) is the base unit for measuring electrical energy. A kW rating is essentially the resulting power output a generator can supply based on the horsepower of an engine. Kilowatt hours (kWh) is the amount of energy you would use if you kept a 1 kW appliance running for one hour. So, if a generator continuously outputs 1 kW of power for 1 hour, 1 kWh of energy is produced.  That is why, the amount of electricity generated is rated in kWh.

A kVA is 1,000 volt amps. A volt is electrical pressure. An amp is electrical current. kVA is used for the rating of an electrical circuit. It is also known as Apparent Power. kVA is the product of a circuit's maximum current and voltage rating. Fundamentally, kVA denotes the value of power (Voltage * Current). It can be calculated dividing Power (P) by Power Factor (PF) i.e. kVA = kW / PF.

Cummins doesn’t just create power solutions, we innovate the power that people can depend on. We’ve been that doing for more than 100 years. With 58,000 employees, 9,000 service and distributor locations, and solutions for 11 industries, we are equipped to deliver on power and technology demands with connected solutions, minimized downtime, and expert support throughout the equipment’s lifecycle. 

As a leader in power technology solutions, our quality products and services range from oil and gas industry to mining to construction to agriculture and more. Above all, Cummins is trusted (14 consecutive years on Ethisphere World’s Most Ethical Companies List), innovative (we created world’s largest PEM electrolyzer and America’s first zero-emissions ferry), dependable (we power homes and industries in approximately 190 countries and territories), and responsible (ranked 24th on America’s Most Responsible Companies List 2021).