Renewable Natural Gas | Cummins Inc.
truck moving towards the sun setting
Meet evolving energy standards with clean and renewable natural gas

Since methane is the main component of natural gas, RNG can be used interchangeably with natural gas derived from fossil fuels and in natural gas engines. Alternative fuels like RNG can help you meet regulations and adopt cleaner energy.

Renewable natural gas solutions by Cummins

Step into the future with Cummins’ portfolio of natural gas engines and generators. Our reliable and efficient solutions are here to move the world forward.

Natural gas engines

Our reliable and efficient natural gas engines provide long-term savings and immediate regulatory compliance.
Technician working on a Cummins generator

Natural gas generators

Cummins natural gas generator sets from 13 - 2,000 kW deliver flexible and sustainable power to a range of industries.

Experience the benefits of adopting RNG

Maintain performance and scalability while reducing GHGs and CO2 emissions with RNG, a cleaner alternative to conventional natural gas and fossil fuels.

Comparable to diesel

RNG delivers similar power and reliability while operating more quietly and with a reduced environmental impact.

Offsets fuel costs

Because RNG can often be produced domestically, RNG offers pricing stability and can help companies eligible for the US EPA’s renewable fuel standard program drive fuel cost savings.

Provides flexibility

RNG helps reduce net carbon emissions while producing heat, generating electricity, and powering your fleet.

Leverages existing infrastructure

Our refueling network eliminates the need to build new infrastructure and enables a seamless transition to RNG.

Renewable natural gas FAQs

RNG is sometimes known as biomethane or upgraded biogas. When biodegradable materials decompose, they release methane and undergo aerobic digestion, a process in which bacteria break down organic matter. This process produces organic materials like biogas, which can be captured and converted into natural gas. With only a minor clean-up and refinement, biogas can generate heat and electricity.

Read More

RNG differs from fossil fuels because it's produced from biodegradable waste. When these biodegradable materials decompose, methane is released. This methane is then captured and converted into RNG. Because methane is the primary component of natural gas, RNG is interchangeable with natural gas derived from fossil fuels.

Watch Now

Methane is the primary component of RNG, which is chemically almost identical to conventional natural gas. However, RNG is carbon-neutral because it originates from fermented organic waste, such as sewage sludge or animal manure. Depending on the energy source, the carbon intensity of RNG can even be sub-zero.

Watch Now

Experts use a carbon negative index to assess the environmental impact of various fuels. A fuel is considered carbon-negative when it reduces the amount of carbon dioxide (CO2) in the atmosphere. The carbon intensity of RNG depends on the type of feedstock used to produce it. This means where the RNG derives from determines its place on the scale and whether or not it's considered carbon negative.

Watch Now

Connect with us