Dinner Cruise Vessel for Chao Phraya River | Cummins Inc.
""
Marine

Dinner Cruise Vessel for Chao Phraya River

by Alan Haig-Brown

Cummins Vessel Reference #726

left to right: Sakchai Rujiphapra, Director, Mahachai Dockyard; Sathit Suwanprasert, Senior Engineer, Marketing Dept., Cummins DKSH (Thailand) and Ku Wee Ming, Manager, Regional Marketing, Cummins Asia Pacific with the newly launched Wonderful Pearl currently being fitted out alongside at the shipyard.

 

Thailand has long been noted for exquisite food and gorgeous boats. In recent years these two have found luxurious expression in the growing fleet of big, low-slung dinner-cruise vessels. In 2005 we reported on a 53×11-meter vessel capable of feeding 400 people at a sit-down buffet. A pair of 640 HP Cummins KTA19 M3 engines powered this vessel.

 

This coming June of 2014 will see the game moved up several notches when the dinner cruise vessel Wonderful Pearl makes her grand entry to the Chao Phraya River from her builders, the Mahachai Dockyard on the Ta Chin River just to the west of the Bangkok. At 65 by 16 meters she is significantly larger, although she adheres to a similar 1.5-meter loaded draft for the shallow river and a 5-meter air draft to clear the river’s several low bridges. The added length and beam allows for an increased in dinner guests to 700 people on two decks. Propulsion power has been increased to a pair of Cummins KTA38 M1 engines each delivering 1000 HP.

With two galley areas, one for international and the other for Thai food, a pair of escalators between decks, a large fountain on the top deck, air conditioning and opulent lighting through out, the boat will have significant electrical requirements. A pair of Cummins KTA19-powered 350 kW generator sets will meet these demands.

 

Restaurant boat 65x16 meters for 700 guests, 1.5-meter draft, propulsion 2x Cummins KTA38 1000 HP each. two KTA19-powered gensets,

 

A thoughtful design allows a performance stage to be shared between the upper and lower decks. Dinners on the upper deck will be in a first class area while the lower deck will enjoy an affordable option. Finishing throughout will be a delight, with hundreds or even thousands of LED lights set into ceiling features and finely crafted wood joinery work. The decks feature beautiful Takien wood imported from Myanmar.

 

In Bangkok, this will be the way to enjoy fine dining while cruising past the iconic landmarks like the Grand Palace, Wat Arun and the many other temples that line the banks of the Chao Phraya River.

 

Haig-Brown photos courtesy of Cummins Marine

 

 

For more information on new building:

 

Sakchai Rujiphapra
Director
Mahachai Dockyard Co. Ltd.
200 Suttivaitee Road, Tachalom District
Samut Sakorn, 74000, Thailand
Phone: 66 034 497296
E-mail: [email protected]

 

For more information on Cummins Marine engines:

 

Sathit Suwanprasert
Senior Engineer, Marketing Dept.
Cummins DKSH (Thailand) Limited
Phone: 66 23017500 | Extension: 7540
Mobile: 081 913 6599
Fax: 02 3330995
E-mail: [email protected]

 

Ku Wee Ming
Manager, Regional Marketing
Cummins Asia Pacific Pte. Ltd.
No. 8, Tanjong Penjuru, Singapore 609019
Office: 65 6265 0155
Mobile: 65 91135899
Office: 65 6266 0432
E-Mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...