Vard and Cummins with Cochin Shipyard PSV | Cummins Inc.
""
Marine

Vard and Cummins with Cochin Shipyard PSV

by Alan Haig-Brown

Cummins Vessel Reference #696

The Sea Titus shortly after launching at Cochin Shipyard. (courtesy of Cummins Korea)

The Sea Tantalus is the first of a series of Vard Group (STX) designed platform supply vessels being built at Cochin Shipyard Ltd in India. The distinctive hull configuration is being built in countries around the world and the Indian version, the first of four from Cohin, is a fine addition.

At 82.2 by 17-meters the Sea Tantalus has a 7.6-meter depth at the main deck. Built to Det Norske veritas (DNV) standards, including “clean notation”, the new vessel employs diesel-electric propulsion. Power is provided by four 1635 HP (1200 kW) Cummins KTA50-DM1-powered electrical generators. These provide power to a wide range of electrical needs of the vessel as well as the twin 2100 mm azimuthing thrusters each of which has a 1600 kW in put requirement.

A media release from the Cochin Shipyard, (http://cochinshipyard.com/news.html),explains that the vessel has been assigned the “clean notation” by DNV to signify the highest levels of environmental compliance. In addition to other environmental friendly provisions, the new PSV is fitted with a ballast water treatment plant to prevent the transfer of harmful aquatic organisms and pathogens.

Other class notations include: COMF for low noise and high comfort in the 28-member crew accommodations, FIRE FIGHTER-1 for fi-fi capabilities, OILREC for the vessel’s oil recovery potential, and LFL* as the vessel can safely carry liquids such as methanol in specialized stainless steel tanks.

With a design speed of 14-knots, the Sea Tantalus has tankage for 1000 cubic meters of fuel, 1050 m3of water and 250 m3 of lube oil. The cargo deck has a 2100-ton capacity. Engines and engine application support was provided by Cummins Korea. The Sea Tantalus, delivered in March of 2013, will be followed by the Sea Titus, currently on sea trials, in the second quarter, the Sea Tortuga in the third quarter and the Sea Triumph in the fourth quarter of 2013. (http://www.deepseasupply.no/newbuildings)


For further information:

Justin Han
Senior Application Engineer,
HHP, Korea & Japan.
Cummins Korea EBU
Mobile: 82 10 3006 0903
Office: 82 2 3420 0962
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...