Strategic Marine’s Compact Crew Boat | Cummins Inc.
""
Marine

Strategic Marine’s Compact Crew Boat

by Alan Haig-Brown

Cummins Vessel Reference #618

Peacock Satu along side in Singapore.

With literally dozens of their high-speed vessels already working, Australian-based Strategic Marine continues production in several shipyards. A recent visit to Strategic Marine’s Singapore shipyard revealed their compact 28 by 7-meter version ready for work while three sisters were taking shape in the building shed.


Cummins Singapore team leader Tan Eng Huat check the genset control panel.

With a molded depth of 2.99 meters the Peacock Satu has capacity for up to 60 passengers and accommodation for eight crewmembers. Tankage is provided for 20,000 liters of fuel and 5,000 liters of water. The aft deck provides 12-meters of length and nearly the full beam for deck cargos. The vessel’s total design deadweight is 13 tons.

A pair of Cummins KTA38-M3 main engines, each producing 1350 HP at 1900 RPM, turn open propellers through Twin Disc MGX669-SC gears with 2.47:1 ratios. The IMO Tier 2 compliant propulsion package will give the vessel a light running speed of 22 knots. The well laid out engine room also contains a pair of Cummins 6BTA(D)M powered 91 kW generator sets. A Cummins 6CTA 8.3-liter engine, generating 430 HP at 2600 RPM, provides 600 cubic meters of water per hour to a SKUM fire monitor mounted on the cabin top aft of the wheelhouse.


For further information:

Jamie Anderson
Marketing and Sales Process Manager
Strategic Marine Pty Ltd
Lot 5 Clarence Beach Rd.
Henderson, WA Australia 6166
Phone: 61 8 9437 4840
Fax: 61 8 9437 4838
E-mail: [email protected]
Web: www.strategicmarine.com

Cummins Sales and Service Singapore Pte Ltd.
8 Tanjong Penjuru
Singapore 609019
Phone: 65 6261 3555

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...