Exhaust Brakes | Cummins Inc.

Performance benefits: Jacobs Exhaust Brake

truck icon

Ideal for light- and medium-performance applications

where retarding is needed, but packaging and costs are significant drivers

puzzle pieces icon

Combine with a Jacobs bleeder brake

or compression release engine brake for enhanced performance in medium- and heavy-duty applications

Jacobs Engine Brakes® and Exhaust Brakes have provided drivers with increased braking performance for decades and the technologies continue to evolve. Today, these technologies even help to reduce emissions. This was first accomplished with variable valve actuation, then with cylinder deactivation, and now with exhaust throttling to help meet emissions regulations. Jacobs has adapted its long-standing, robust exhaust brake technology for thermal management use for modern commercial vehicle engines, while still retaining its well-known capability as a retarding device.

How Jacobs Exhaust Brake Works

The Jacobs® exhaust throttle works by actuating a flap downstream of the turbo to increase exhaust backpressure and reduce mass flow through the engine. Used alone, the exhaust brake provides light retarding when exposed to the increased backpressure by increasing the work of the piston during the exhaust stroke.

Technologies reducing emissions

thermometer icon

Thermal management device

that effectively increases the workload on the engine and reduces mass flow through the exhaust to increase the enthalpy applied to the catalyst

cloud leaf environmental icon

Use as a fast warm-up or keep-it-warm device

to significantly reduce the engine's nitrogen oxide (NOx) output

hand with lightbulb icon

Def-resistant systems

available for dual dosing applications where the diesel exhaust fluid (DEF) has not fully decomposed before it comes into contact with the throttle

The Jacobs Exhaust Brake® works well for thermal management by increasing the enthalpy applied to the aftertreatment catalyst(s). Next-generation aftertreatment systems can include a dual dosing strategy with a diesel exhaust fluid (DEF) injector located as close to the turbo as possible. This makes it difficult to use an exhaust brake because the DEF will not be fully decomposed by the time it contacts the throttle. Our innovative DEF corrosion-resistant exhaust throttle can be used in these systems without function degradation.

Form

Let's talk about your program

Our engineers are always available to discuss your current or future technology challenges. Contact us using this form, and a member of our team will contact you within two business days.