Commercial natural gas engine service & maintenance schedule | Cummins Inc.

Maintaining and servicing commercial natural gas engines

Originally published September 2023; Updated June 2026

By Mark Ulrich, Director - Customer Support

two semi trucks parked

Summary

Natural gas engines offer lower operating costs and reduced emissions compared to diesel, and their simpler, maintenance-free exhaust treatment system eliminates the filter changes and replacements that diesel engines require.

However, natural gas engines are less forgiving than diesel when maintenance intervals are missed, particularly oil drains, making it critical to track engine hours rather than miles alone, especially in vocational and transit applications with high idle time. Facilities and mechanics servicing natural gas vehicles need only supplemental training and specific safety measures, as the maintenance closely resembles that of traditional vehicles.

Learn best practices for natural gas engine maintenance, including service intervals, spark plug care, oil specs, and how it compares to diesel.

 

Natural gas engines vs. diesel engines maintenance and service comparison

Category Natural gas engines Diesel engines
Exhaust treatment Passive, maintenance-free, three-way catalyst. No DEF or regenerations needed Requires an active system to filter soot and reduce NOx. Diesel particulate filters clog and must be cleaned/replaced
Emissions & cleanliness Very low NOx, virtually no soot. Intrinsically clean combustion.  Final NOx reduction completed in three-way catalyst Diesel combustion produces soot and higher NOx. Requires post-combustion treatment that catches and burns the soot and uses DEF to reduce the NOx
Service intervals The X15N brings longer and more robust service intervals. Historically service intervals have not been as forgiving when intervals are missed, especially oil drains Longer service internals
Operating costs Reduced operating costs compared to diesel due to lower cost fuel Higher operating costs when compared to low cost natural gas
Spill & handling risk Gaseous and dissipates quickly so it cannot be spilled. No residue left on clothing or surfaces Liquid that can be spilled. May leave residue on clothing or surfaces
Maintenance tracking Track by engine hours (not just miles) due to high idle time in vocational/transit use Miles-based tracking is common. Same software tools work for both engine types
Ignition system Spark plugs required (use OEM-approved only, correct torque and no gap adjustments) No spark plugs required (compression ignition)

 

Natural gas engines have a maintenance-free exhaust treatment system

A major benefit of natural gas engines is that they do not require a complicated exhaust treatment system. In diesel vehicles, these systems are used to treat post-combustion gases by filtering out soot and reducing NOx emissions. Over time, the filters clog and must be cleaned or replaced to ensure performance. 

Natural gas engines are, in contrast, intrinsically clean. They produce very little NOx and virtually no soot, so only light exhaust aftertreatment is needed. Cummins’ engines use a maintenance-free three-way catalyst exhaust treatment system, eliminating the need for filter changes or replacement of exhaust control systems. This reduces the cost and complexity of maintenance and decreases fleet downtime. 

Natural gas engine best maintenance practices

When maintaining a natural gas engine, there are several best practices that need to be kept in mind. First, it’s important to factor in idle time to the maintenance schedule. That’s why it is recommended to track hours on the engine and not just miles driven when tracking maintenance intervals. This is especially important to keep in mind with vocational and transit applications given the high level of idle time inherent to those duty cycles. 

Using genuine Cummins parts such as spark plugs and oil, can significantly reduce unexpected issues and downtime of natural gas vehicles. All Cummins components have undergone validation to ensure they meet the company's design standards and emission certifications. 

Low pressure fuel filters should be drained regularly as a routine maintenance practice. This is a quick process that involves loosening the filter and allowing the fuel to drain out. This helps to protect the engine and allows for the identification of any issues in the compressor. 

Checking for the latest ECM calibration at every spark plug change is also recommended. These calibrations are typically released once or twice a year. If a fleet has already invested in software tools for updating diesel engines, the same tools can be used for natural gas engines.

Natural gas engine maintenance components

Component Interval Notes
Engine oil (CES 20092) Track by engine hours Cummins/Valvoline spec oil compatible with diesel, natural gas, and gasoline engines. Critical to complete service intervals
Spark plugs Per OEM service schedule Use manufacturer-approved spark plugs only. Use correct torque and keep clean. There should be no gap adjustments needed
ECM calibration At each spark plug change Released once or twice per year. Same software tools as diesel engines
Low pressure fuel filters Drain regularly Quick process that helps identify potential compressor issues
Crankcase breather Per recommended service schedule Missing service intervals may contribute to engine problems
Ignition coil extension Per recommended service schedule Missing service intervals may cause damage to catalyst and coil extension
Standard coolant Per recommended service schedule Missing service intervals may cause front or rear main seal leaks
Coolant filter Per recommended service schedule Part of regular fluid maintenance

 

It’s critical to follow recommended maintenance intervals for natural gas engines

Natural gas engines aren’t as forgiving as diesel engines when it comes to missing service intervals, especially oil drains. Cummins has put significant effort into educating fleets over the years about the best way to track the time on the engine to make sure the right intervals are being met, whether engine hours or miles driven is the primary metric being used. 

The CES 20092 spec oil is the recommended oil for spark ignition engines and is the result of a joint effort by Cummins and Valvoline. This oil can be used on diesel, natural gas and gasoline engines.

It is also important to replace the spark plugs per the recommended service schedule. During installation, care should be taken to maintain the cleanliness of the spark plugs and to install them using the correct torque. Only manufacturer-approved spark plugs should be used as they are extensively tested and certified for each engine. Aftermarket spark plugs haven’t been proven to meet the emissions certifications. You also should not adjust the gap on your new spark plugs or check the gap with a friction gauge. If a new spark plug appears to be out of spec, return it for a replacement.

The following table shows the recommended maintenance intervals for several additional components. These include crankcase breather, ignition coil extension, standard coolant and coolant filter. 

chart of general engine maintenance requirements
chart of general engine maintenance requirements

Failure to follow these maintenance intervals may lead to engine problems. These potentially include misfire, damage to the catalyst and ignition coil extension, front or rear main seal leaks and even piston failures. In case of any such issues, fleet owners should reconsider their maintenance schedule and ensure maintenance is being performed on time.

Since its 2024 launch, the Cummins X15N has moved natural gas into scaled fleet adoption, with expanding orders from both early adopters and new-to-fuel fleets. With this natural gas engine, Cummins is working on synchronizing maintenance intervals to allow users to complete more service events at once. Below you’ll find the X15N maintenance intervals.

X15N Maintenance intervals chart
X15N Maintenance intervals chart

Natural gas vehicle facilities and mechanics

Facilities that service natural gas vehicles require specific safety measures to prevent potential safety hazards. Ventilation, path control, space heating, electrical wiring, equipment installation, and methane detection and control systems are some of the safety measures that need to be taken. For additional safety questions, fleets can connect with their local Clean Cities coordinator. 

Experienced mechanics require only supplemental training to work on natural gas vehicles, since their maintenance closely resembles the maintenance of traditional vehicles. There are examples of fleets that run a combination of diesel and natural gas engines. Fleets with large numbers of natural gas vehicles often keep natural gas and diesel maintenance separate for efficiency. However, maintenance for both natural gas and diesel vehicle is possible at the same premises if there is at least one dedicated bay with the appropriate safety considerations for natural gas systems. The joint venture between Cummins and Rush Enterprises will provide customers with a service network through Rush Truck Centers’ dealerships and Cummins’ distributors. With over 250 locations in the US and Canada, both companies' networks will be equipped with certified technicians and a comprehensive natural gas vehicle parts inventory.

Unlike diesel, natural gas cannot be spilled. Any leaking natural gas, being in gaseous form, will quickly dissipate, and will not soak gloves or overalls, or leave residues on surfaces. Maintenance crews may have a more pleasant experience working on a cleaner, soot-free engine. 

Frequently asked questions

  • Track engine hours (not just miles) to ensure the right maintenance intervals are being met
  • Follow recommended service schedule intervals strictly, as natural gas engines are not forgiving when intervals are missed
  • Check for the latest ECM calibration at every spark plug change
  • Drain low pressure fuel filters regularly to identify issues in the compressor early
  • Use genuine Cummins parts to reduce unexpected issues and downtime

Natural gas engines use a maintenance-free three-way catalyst system, eliminating the need for filter changes or exhaust control replacements that diesel engines require.

No. Natural gas engines produce very little NOx and virtually no soot, making them intrinsically clean.

By engine hours, not just miles driven, especially important for vocational and transit applications that have high idle time.

No. Natural gas engines are not as forgiving as diesel engines when maintenance intervals are missed, particularly oil drains.

Author Profiles

Mark Ulrich

Mark Ulrich, Director - Customer Support

With 30 years at Cummins, Mark Ulrich has built extensive expertise across product development, testing, and customer support. As Director of North American Customer Support, he leads a team dedicated to delivering technical solutions and support for customers across the Cummins Engine Business.

Want to find out more?

Receive the latest from Cummins in technologies, products, news, and insights.