Cummins Power for Peruvian Purse Seiner | Cummins Inc.
""
Marine

Cummins Power for Peruvian Purse Seiner

by Alan Haig-Brown

Cummins Vessel Reference #701

The Ana Lucia ready to fish.

 

“We are a 100% Peruvian company with a fishing tradition and entrepreneurial spirit. Our knowledge, transmitted from one generation to the next, originates from the direct experience of people closely linked to the sea and has been consolidated by the professionalism and commitment of a team of experts which works in each one of the branches of the company.” So says the web page of the Peruvian anchovy fishing company Hayduk Corporation.

 

 

 

Hauling the seine.

 

The company web page goes on to say, “The future presents itself to us as a world to conquer and we face it with major projects and placing ourselves in a leading position in tendencies and technology, always maintaining our essence as a company: as fishermen and Peruvians.”

 

An example of this commitment to maintaining a leading position in technology was demonstrated recently with the repower of one of their anchovy purse seiners with a modern Cummins KTA50 M2 main engine. The Ana Lucia is a 48.95 by 9.05-meter purse seiner with a 500-ton cargo capacity. As part of the company’s fleet of about 22 purse seiners, they also have six trawlers fishing hake, the Ana Lucia is an important contributor of anchovies both for direct human consumption and indirect human consumption by way of fish meal. This carefully regulated fishery is an important contributor to the Peruvian economy.

The repower of the Ana Lucia involved the removal of a Cat 3516 rated for 1600 HP at 1200 RPM and its replacement with the Cummins KTA50 M2 rated for continuous duty of 1600 HP at 1800 RPM. In order to keep the same four-blade 2166 m/m by 1748.94 propeller, that is optimized for the vessel, it was necessary to also change the gear from one with just under a 4:1 ratio to a Masson –ZF W7300 with a 6:1 ratio. This allowed for the significant increase in RPM with the new engine. With the new engine in place and general servicing, the Ana Lucia makes 12.5 knots running light and 11.5 knots with a full load.

 

 

In the shipyard.

 

Photos courtesy of Distribudora Cummins Perú SAC

 

 

For further information:

 

Hugo Huayanca Valverde
Lider de Mercado
Distribuidora Cummins Perú SAC
Tel: 511 614 7979 Extension: 8463
Cell: 99754 7811
E-mail: [email protected]
Web: www.cumminsperu.pe

Olmedo Farfan
Marine Business Leader – Latin America
HHP Marine Business
4500 Leeds Ave.
Charleston, SC – USA
Tel: 843 745 1581
Cell: 843 298 4580
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...