Dann Marine: Family Pride, Fleet Pride | Cummins Inc.
""
Marine

Dann Marine: Family Pride, Fleet Pride

by Alan Haig-Brown

Cummins Vessel Reference #606

 

Dann Marine Towing (www.Dannmarinetowing.com) shows the pride in five generations in the marine business by maintaining their fleet of 17 tugs in an exemplary state of readiness. The firm operates out of their base in Chesapeake City, Maryland and tows along the Atlantic and Gulf coasts as well as South and Central America. The company pride is also demonstrated in their participation the American Waterways Operators, Responsible Carriers Program.

 

Maintaining and building a good fleet requires upgrading and repowering. Dann Marine has recently put their 100 by 32-foot tug Gulf Coast back into service following a major refit that included swapping out a pair of a competitor’s 1200 HP engines in favour of a pair of 1600 HP Cummins QSK50 engines. The repower involved modifications to the engine foundations and cooling system all of which was carried out at the Lyon Shipyard in Norfolk, Virginia. The shipyard also has an extensive history having been founded in 1928 by George C. Lyon.

The ABS load-lined model bow tug is fitted with an Intercon DD200 towing winch loaded with 2000 feet of 2-inch cable and 305 feet of 1.5-inch wire. It carry tanks for 81,385 US gallons of fuel and 5,268 gallons of potable water.

 

For further information:

 

Robert Dann Jr.
Dann Marine Towing, Inc.
299 Boatyard Rd.
Chesapeake City,
Maryland, US
Phone: 410 885 5055
E-mail: [email protected]
Web: www.Dannmarinetowing.com

Richard Sutton
Cummins Power Systems, LLC
Baltimore, Maryland
Phone: 410 762 1419
Mobile: 410 690 2986
E-mail: [email protected]

Lyon Shipyard
1818 Brown Ave.
Norfolk, VA 23501-2180
Phone: 757 622 4661
Web: www.lyonshipyard.com

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...