Dongara Marine Ferry | Cummins Inc.
The 24 X 5.5-meter Cummins Powered MV Tricia on sea trials
Marine

Dongara Marine Ferry

by Alan Haig-Brown

The 148-seat MV Tricia alongside on delivery tripPlacing a board deck across two canoes, to make a broad flat and stable surface for transporting passengers and freight, was often done to form early ferries. The true catamaran is an evolution of that practical design concept. In recent decades, Australia has led in the development of all shapes and sizes for aluminum catamaran ferries.

In December 2019, Dongara Marine of Port Denison delivered a very practical 148-seat, 24 by 5.5–meter ferry to Western Australia’s Public Transport Authority. The MV Tricia, has joined two similar, but slightly smaller, ferries on a run of about 1.5 kilometers between Elizabeth Quay and Mends Street Jetty in South Perth.

One of the two 184 kW Cummins QSB6.7 main enginesPragmatically designed as a people mover in protected waters, the craft is given an attractive over all superstructure. A piloting console is set forward in the cabin on the starboard side to allow the master to make landings single handed. Passenger entry is from the starboard side. The catamaran is built to drawings from Dongara Marine’s design partner, Southerly Designs, who have an impressive portfolio of sea kindly fishing and pilot boats, many of which were also built by Dongara Marine.

The starboard side operator stationThis quality design and fabrication history of the two firms is evident in the MV Trica. A pair of 184 kW Cummins QSB6.7 engines turning fixed pitch five-blade Veem props provide propulsion power through Twin Disc MGX5065 gears. With a 16-knot design speed, the vessel easily achieved that on sea trials. A pair of electric bow thrusters increases the vessel’s maneuverability alongside the dock making handling possible with a single operator. The main engines were supplied by Cummins South Pacific in Perth. The MV Tricia is built to AMSA NSCV 2E class requirements.

Download QSB6.7 Spec Sheet

Photos courtesy of Dongara Marine

For further information: 

Rohan Warr
Managing Director
Dongara Marime
2 Carrol St. 
Port Denison, 
WA 6525, Australia
Email: [email protected]
or
Andrew Jeffs
Communications
Dongara Marine
E-mail: [email protected]
Phone: +61 8 9927 2257
 
Peter Brookes
Cummins South Pacific
3 Reid Rd, Perth Airport
Western Australia, 6105
Phone Dir: +61 8 9475 8721
Cell: +61 (0) 409 100 128
Email: [email protected]
 
Jennifer McQuilken
Marketing Communications, Marine and Oil & Gas
Cummins Inc.
4400 Leeds Ave. Suite 300
Charleston, SC 2940
E-mail: [email protected]
Phone: +1 843-696-9534 (call or text)

Alan Haig-Brown
A. Haig-Brown & Assoc. Ltd.
Bangkok, Thailand & Vancouver, Canada
Phone: 66 (0)8 5347 6206
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...