Repower of the Tug Gretchen H | Cummins Inc.
Cummins’ QSK 19 Powered Tug- Boyer Gretchen
Marine

Repower of the Tug Gretchen H

by Alan Haig-Brown

Cummins’ QSK 19 installed- Gretchen’s engine roomAs sometimes happens with boats in the maritime world, the recent repower of a tug shone a light on a pair of well-known independent companies. The tug Gretchen H. (ex Harry Olsen, Polar Breeze) was built by Rodriguez Shipbuilding of Coden Alabama in 1997 and is currently owned, since 2005, by Boyer Towing.

The Gretchen H is a good solid boat and her owners decided she was well worth a new set of engines. At 80 by 30 feet she has an eleven-foot depth. As with many tugs out of the Rodriguez yard she has triple propellers and triple engines. She had an older set of engines rated at 700 HP each. The owners decided on three new Cummins QSK19 Tier 3 compliant engines rated for 750 HP each at 1800 RPM. The existing Twin Disc MG5202DC gears with their 6.1:1 ratio were a good fit for the new engines so they were retained.

Boyer Gretchen Wheel HouseBoyer did the repower themselves at their own Seattle yard.  The old Luggers came out and the new, bright-red Cummins machines went in. The tug performed flawlessly on sea trials at the end of January and is ready to go back to work towing barges between Seattle, Wake Island, or Alaska.

 

Photos: Mike Fourtner/Cummins

Download QSK 19 Spec Sheet

For further information:

Boyer Towing
Seattle, WA
206 763-8688
 
Mike Fourtner
Commercial Marine Sales, Pacific Region
Cummins Sales and Service
3300 Mottman Rd. SW
Olympia, WA 98512
Direct     360 242 4175
Mobile:  360 742 2864
Email: [email protected]
 
Capt. Jennifer McQuilken
Marketing Communications Leader, Marine and Oil & Gas
Cummins Inc.
4400 Leeds Ave. Suite 300
Charleston, SC 29405
USA
E-mail: [email protected]
Phone: +1 843 696-9534 (call or text)

A. Haig-Brown & Assoc. Ltd.
Bangkok, Thailand
Phone: 66 (0)8 5347 6206
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...