oil drilling engineers on rig
Drilling

Independence Contract Drilling

Customer-Inspired Solutions
by Cummins Inc., Global Power Technology Leader
Project: Dual Fuel Unit Engineering, Manufacturing, Testing and Support
Location
Houston, Texas, USA
Date
Styczeń 2018

Customer testimonial: Independence Contract Drilling

Two years ago, Independence Contract Drilling (ICD) decided to make a strategic shift, leveraging external expertise and economies of scale available from component manufacturers in the design and construction of their rigs. This included outsourcing both the drilling power module and skidded assemblies, with the decision based on a potential partner’s ability to work with ICD from design through manufacturing and testing, then following through with a complete support strategy.

Application: 1500-hp Drilling Rigs
Project: Dual Fuel Unit Engineering, Manufacturing, Testing and Support
Results: Industry-Leading Uptime, With Instantaneous 0%-100% Ramp-Up

Several factors were instrumental in the decision to choose Cummins. First, Cummins demonstrated an ability to listen carefully to ICD’s input, and custom-design solutions that met its drilling power module specifications. Second, a detailed cost analysis on projected maintenance expense savings and life-to-overhaul projections convinced ICD of the value proposition. Cummins also demonstrated to ICD the ramp-up capabilities of the Cummins engine with respect to load changes and the Modular Common Rail Fuel System (MCRS). But it was the seamless coordination between the Cummins Houston Center Of Excellence (COE) and the local Cummins distributor – Cummins Southern Plains – ensuring that Cummins would be fully invested in maintaining and enhancing equipment uptime and productivity for ICD that clinched the deal.

Watch the video below to see the Cummins – ICD story and the incredible results. You can also read the case study brochure for more information:

Independence Contract Drilling case study brochure

Customer Inspired Solutions: Independence Contract Drilling

The engines have been proven. The support staff have proven themselves. The engineering work has proven itself. And the engines have exceeded anything I ever thought.

Lance McDonald, Director of Rig Assembly