Driven by power. Defined by reliability

Tier 4 rental generator sets
Built for uninterrupted performance

At Cummins, we know that your operations demand more than just energy — they require certainty. Our rental power solutions combine cutting-edge engineering with unwavering dependability, providing seamless performance even under the most challenging conditions. With every unit, you gain not only power but the confidence that your project, site, or facility will never be left in the dark. Because true reliability isn’t just a feature — it’s our promise.

Explore brochure

Rental power applications

Audience at an event

Events

Whether it be a music concern or a major sports game, Cummins enable events to run smoothly with no power interruptions.

Workers inspecting industrial equipment

Industrial

In industrial settings, Cummins support construction and mining and oil and gas extraction and can even be incorporated into microgrids.

Crew defending their ground

Military and Institutions

Reliable and uninterrupted power for bases and permanent installations as well as hospitals and other mission-critical facilities.

Overhead view of a water treatment facility

Utilities

From base load to emergency backup and peaking power, Cummins supply utilities like wastewater treatment with the power to run seamlessly.

Massive flood

Emergency power

When crises like natural disasters occur and utility power fails, Cummins provides the vital emergency power to support people in need.

Utilizing solar and wind power together

Hybrid power

Cummins rental power solutions can be used in conjunction with new energy solutions to provide reliable and more sustainable hybrid power.

Key features and benefits

To view full features and benefits, visit the North America rental power solutions brochure via the link below.

US EPA Tier 4 final certified Cummins engine and aftertreatment system

Bigger capacity fuel & DEF Tank with containment (dual wall 110%+ spillage) basin

Auxiliary fuel connections

Cummins PowerCommand® 3.3 control on most models

Cooling system rated at 50°C at 100% standby

Warranty 1 year unlimited hours or 3 years — 3,000 hours

Hydrogen building blocks

You have 4 tier questions

The EPA’s Tier 4 regulations are frequently a source of confusion for those who rely on large stationary generators for backup and prime power uses. Owners and operators of these generator sets (gensets) have many questions about the EPA’s emission standards and what the implications mean to them.

Cummins has the answers

We work closely with the EPA to fully understand every subsequent change to their regulations as they implement ever cleaner air standards. Cummins was the first manufacturer to introduce EPA Tier 2 and Tier 3 generators to the market, well ahead of the regulatory deadline. Our commitment to providing you with total operational flexibility in how you choose to use generator power is what drives us to stay ahead of the game.

We were the first manufacturer to offer a full range of Tier 4i-certified gensets, and the first to receive Tier 4F certification when the EPA began issuing certificates in January 2014.

Talk to the team

If you have questions, fill out the form below and we’ll be in touch.

CAPTCHA
To pytanie sprawdza czy jesteś człowiekiem i zapobiega wysyłaniu spamu.
Connect with us