Dutch Vessels Continue to Set Standard | Cummins Inc.
""
Marine

Dutch Vessels Continue to Set Standard

by Alan Haig-Brown

Cummins Vessel Reference #573

The Elja-V coming alongside on a serene waterway. Photo courtesy of Cummins Holland.

Following in a long tradition, the shipyards of the Netherlands continue to produce immaculate inland river vessels. In recent years these have tended to be built on hulls shipped from the cost-effective shipyards of China to be finished to the highest standards in Dutch shipyards.

Last year, the shipyard of De Groot in Dordrecht completed the MS Elja-V for Ellie and Jacob Van der Vlag. With 35 years sailing together this is the couple’s sixth vessel with the name Elja-V. At 110-meters in length the new vessel has the standard 11.45-meter beam for navigation on the Rhine, Mains and Danube. This size also allows for the stowage of the family’s two cars on deck aft of the hydraulically raised and lowered wheelhouse. Power for the vessel is provided by an electronically-controlled Cummins QSK50-M engine producing 1194 kW (1600 HP) at 1800 RPM. This Tier 2 engine meets the current emission standards for Europe’s inland waterways. The ship is also fitted with a Cummins QSK15-C bow thruster delivering 530 HP at 1800 RPM for maximum control of the Elja-V in the inland waterway locks. Electrical needs for the vessel, including the comfortable living accommodation, is met by a pair of Cummins 4BT3.9-B4 powered 64 kVa generators.


China-built hulls being off loaded in Rotterdam. A. Haig-Brown photo

An indication of how seriously the families that travel Europe’s inland waterways is the ultra-comfortable in-floor heating system for both the accommodations and the wheelhouse. No matter how far into the more mountainous regions of Europe, even over the divide and down the Danube, they may travel, the Van der Vlag family will enjoy the quality to which they are accustom in the Dutch lowlands.


For further information please contact:

Sjoerd Spronck
Advertisement & Promotion
Scandinavia and Benelux
Cummins Holland B.V.
Olivijn 800
3316 KH Dordrecht
The Netherlands
Tel: 31 78 6530 927
Fax: 31 78 6176 579
E-mail: [email protected]
Web: www.cummins.com | www.cummins.nl

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...