New Zealand’s Q-West To Built High-Speed Ferry | Cummins Inc.
""
Marine

New Zealand’s Q-West To Built High-Speed Ferry

by Alan Haig-Brown

Cummins Vessel Reference #713

A rendering of Q-West's current build project.

As with most island nations, New Zealand is heavily dependent on ferries. By this time next year, there will be a new ferry added to the Auckland-based Fullers Group fleet. Currently being constructed at Q-West Boat Builders Ltd. on the Wanganui River, the Incat Crowther-designed catamaran will join a large number of aluminum vessels launched from this versatile yard. (http://www.q-west.com/recently-completed/all-boats)

At 34 by 9.5-meters with a molded depth of 3.05-meters this will be among the larger vessels delivered from this yard. With a capacity for 338 passengers, 256 inside and a further 82 external, this will be a capable people carrier. The owners have an existing fleet of ferries providing service to islands in the Hauraki Gulf outside of Auckland Harbour on the North Island.

A pair of Cummins QSK38-M engines, each delivering 1400 HP at 1800 RPM to ZF gears and Tiger 5-blade 44.5-inch propellers, will provide propulsion for the catamaran . This will give the ferry an operational speed of 26 knots. A pair of Cummins 6B-powered 100 kVA generators will provide electrical service.

A Palfinger PK4501M deck crane will handle cargo and stores. Tankage will be provided for 8,000 liters of fuel and 3,000 liters of water.


Renderings provided by Q-West:


For further information:

Colin Mitchell
General Manager
Q-West Boat Builders
P.O. Box 862,
2a Gilberd St.
Wanganui,
New Zealand
Phone: 64 6 349 0035
Fax: 64 6 344 3592
E-mail: [email protected]

Matt Lyon
Incat Crother
NSW, Australia
Phone: 61 2 9450 0447

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...