Blessey Marine: Rollin’ On The River | Cummins Inc.
""
Marine

Blessey Marine: Rollin’ On The River

by Alan Haig-Brown

Cummins Vessel Reference #635

MV Steve Scalise

The demand for handy sized towboats to handle inland river tows continues to grow and one of the strongest contributors to that growth is Blessey Marine. Primarily handling petroleum-related products, the firm has grown rapidly to their present fleet size of over 60 vessels with more on order. Although they have vessels ranging from 700 to 4900 HP, the 2000 HP Class is proving popular. Two recent deliveries illustrate slightly different sizes and configuration of their 2000 HP towboats.



The MV Steve Scalise was built at the Verret Shipyard in Plaquemine, Louisiana to a design by the shipyard. Delivered in early 2011, the 85 by 30-foot towboat is a little longer than some of this horsepower class. With a molded depth of 10.5-feet the hull has tankage for 30,000 gallons of fuel, 16,800 gallons of water and 450 gallons of lube oil. A pair of EPA Tier 2 compliant Cummins K38-M main engines turn four-blade 74 by 56-inch four blade stainless propellers from Sound Propeller through Rentjes Model 562 gears with 6:1 reduction.


MV Jerry "Dog" McLain

The MV Jerry “Dog” McLain was also delivered this year. This towboat, from by the Raymond and Associates yard in Bayou LaBatre, Alabama, was also built to the shipyards own design. At 76-feet the “Dog” is shorter than the Verret boat by nine feet. However with a 35-foot beam she has five-feet more width. The slightly deeper, 11-foot molded, hull carries 31-300 gallons of fuel, 10,300 gallons of water and 587-gallons of lube oil. The engine room has the same power set with two Cummins K38 main engines. The difference is in the TwinDisc MG540 gears with 7:1 rations swinging Kahlenberg Stainless Steel four-blade 76 by 63-inch wheels.

Both vessels have Patterson deck winches, Hiller Fire Suppression systems and a pair of Cummins 6BT5.9-powered 85 kW Stanford generators. The Scalise is fitted with a Blue Box Recording System and the Jerry “Dog” Mclain has Simplex Shaft Seals and a Sims Motion Detector. The Scalise has accommodation eight people while the “Dog” has bunks for seven.

Assigned to inland towing both vessels are inspected under the Un-Inspected Towing Vessel Program (UTV) by the US Coast Guard.

Photos courtesy of Blessey Marine

For further information:

Jim Clendenon
V.P.o fNew Construction, Repair and Maintenance
Blessey Marine
1515 River Oaks Rd. East
Harahan, LA 70123
Phone: 504 734 1156
Web: www.blessey.com

Verret Shipyard
29120 Hwy 75
Plaquemine, LA 70764
Phone: 225 659 2647

Raymond & Associates
14584 Shell Belt Rd.
Bayou LaBatre, AL 36509
Phone: 251 824 2152

Al Heisler
Cummins Mid-South Inc.
110 East Airline Hwy
Kenner, LA 70062
Phone: 504 468 3535
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...