New Patrol Boat for Indonesia | Cummins Inc.
""
Marine

New Patrol Boat for Indonesia

by Alan Haig-Brown

Cummins Vessel Reference #593

 

Since 1980, PT Dumas Tanjung Perak Shipyard in East Java has build dozens of vessels for various departments of the Indonesian Government. Their most recent delivery, the Hiu Macan Turul 401, was designed and built for the Department Kelautan Dan Perkanan.

 

The vessel’s 42.5 length and seven-meter beam provides accommodation for up to 18 people. Propulsion power is provided by two Cummins QSK60-M engines each producing 2500 HP at 1900 RPM. The engines turn into Twin Disc MGX 5600 gears with 3.51:1 ratios. The boat’s 1540 by 1659 m/m propellers were provided by Singapore’s Asia Foundry.

 

For further information:

 

Mr. Suryanto,
Department Kelautan Dan Perikanan,
Indonesia
Phone: 6221 350 3458

P.T. Dumas Tanjung Perak Shipyard
JL. Nilam Barat 12,
Surabaya, 60177
Indonesia
Phone: 62 31 329 5111
Fax: 62 31 329 3240
E-mail: [email protected]

Yoseph T. Arifin
Cummins Diesel Sales Corp.
8 Tanjong Penjuru,
Singapore 609019
Phone: 65 6661 8265
Fax: 65 6266 0432
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...