INSITE CENSE™
Chat with Support

INSITE CENSE™

This is an enhanced engine protection feature. CENSE™ engine monitoring (with standard engine shutdown log) is incorporated into the upgraded engine ECM, eliminating the need for an additional diagnostics module or an Exhaust Gas Temperature (EGT) converter box.

 

INSTALLATION INSTRUCTIONS

  • This tool will only function on versions of Windows 7 32-bit (or prior versions).
  • The software install package is NOT compatible with Update Manager.
  • The software must be manually installed. The instructions are included in the below zip file. Please follow the provided instructions to ensure the software is properly installed.
  • This tool also requires INSITE 8.X to perform calibration downloads to the CENSE RS-232 modules.

 

SOFTWARE DOWNLOADS

INSITE for Cense (RS-232)

File Name: INSITEforCense.zip

File Size: 31 MB

DOWNLOAD

 

Search Digital Products & Services Support