Farmer Cuts Cost with Cummins Genset Fuel Economy | Cummins Inc.
275 kVA genset is designed  around Cummins’ electronic  QSL9 engine, a proven winner.
Agriculture

Farmer Cuts Cost with Cummins Genset Fuel Economy

by Cummins Inc., Global Power Technology Leader

Pricing plays big role in choosing Cummins for mains power

NSW Riverina farmer Ken Brain has achieved more than a 50 percent cost reduction through switching from mains electricity to Cummins diesel generator power for irrigation pumping.

Ken Brain (right) with Cummins sales executive Adrian Melotto (left)  and Pumps, Pipes and Power owner John Byrne.
Ken Brain (right) with Cummins sales executive Adrian Melotto (left) and Pumps, Pipes and Power owner John Byrne.

Early in 2017, Brain acquired a property that was set up with mains power to drive a 100 kW line bore pump.

The decision to switch to diesel generator power came after he priced both options, with mains power calculated at $76/megalitre and the Cummins diesel generator at $32/megalitre. The result is a saving of thousands of dollars a year. “I’m very happy,” says Ken Brain in a classic understatement.

Ken and wife Wendy farm 3440 hectares (8,500 acres) in the Coleambally region – corn, rice and soya bean in the summer and wheat, manola and barley in the winter.

Cummins QSL9 diesel generator… saving thousands of dollars a year.
Cummins QSL9 diesel generator… saving thousands of dollars a year.

Looking to cut costs with diesel-powered genset

“The cost of mains electricity is a killer… the access charge alone is $1000 a month,” says John Byrne, principal of Coleambally-based Pumps, Pipes and Power who advised Ken Brain on the benefits of using a Cummins generator set.

As a business owner and also a farmer, Byrne has an intimate knowledge of the cost pressures facing people on the land. Byrne uses a Cummins genset on his own farm for irrigation pumping and knows exactly the cost benefit.

“Ken came to me wanting to know what could be done to cut costs,” says Byrne. “My advice was that a diesel genset was the best option, and that has proved to be the case.”

The 275 kVA genset on Ken Brain’s property is designed around Cummins’ electronic QSL9 engine, a proven package in terms of performance, reliability and fuel efficiency and a perfect fit for Brain’s pumping requirements – around 11 megalitres a day which are pumped into a dam.


QSL9 engine's fuel economy right in the sweet spot at 16-17 litres/hour

“We were expecting the QSL9 to use in the high 20s (litres/ hour) but in actual operation it’s a lot less which is brilliant,” says Byrne. Ken Brain confirms that consumption is only 16-17 litres/ hour with the Cummins running at 1500 rpm, right in the ‘sweet spot’ for best fuel economy.

Cummins’ reputation for technical and aftersales support figure strongly in John Byrne’s business approach. He works closely with Cummins Wodonga sales executive Adrian Melotto to develop packages that deliver both performance and fuel efficiency for irrigation pumping, while the Cummins Leeton branch is well placed for service support.

Related case studies
Agriculture Case Study

Cummins CustomPaks are being used for water management as Thailand struggles with its water crisis Sixty Cummins CustomPaks are in service in Thailand a...

Agriculture Case Study

The search for improved fuel economy and reliability were the key reasons Matthews Transport selected the 15-litre Cummins ISXe5 in 2013 as its standard engine ...

Agriculture Case Study

Australia’s only cotton seed supplier, Cotton Seed Distributors (CSD) has partnered with the CSIRO for a number of years developing improved cotton varieties ...