New Zealand’s Q-West Delivers Catamaran Ferry | Cummins Inc.
""
Marine

New Zealand’s Q-West Delivers Catamaran Ferry

by Alan Haig-Brown

Cummins Vessel Reference #747

A fine new vessel from Q-West.

Q-West Boat builders, located in Wanganui have delivered an Incat Crowther-designed catamaran to the Auckland ferry operator Fullers Group. The 34 by 9.5-meter commuter ferry will operate out of Aukland on a number of different routes. With seating for up to 338 passengers the ferry, named Te Jotuku’, can also carry some freight on her foredeck.

 

A well laid out bridge console.

A pair of Cummins QSK38-M mains, developing 1400 HP each at 1800 RPM, turn 44.5-inch, five-blade propellers through ZF gearboxes powers the all aluminum vessel. This combination gives a cruising speed of 26 knots. With a molded depth of just over three meters, the ferry draws only 1.9-meters of water.

 

Seating over 300 passengers.

For more specifications see: http://www.q-west.com/recently-completed/te-kotuku

For the owner see: http://www.fullers.co.nz/

Photos courtesy of A-West

For more information:


Colin Mitchel
General Manager
Q-West Boat Builders
P.O Box 862
2A Gilberd St.
Wanganui,
New Zealand,
Phone: 64 6 349 0035
E-mail: [email protected]
Web: www.q-west.com

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...