Cummins Case Studies

We’re in it for the long haul. We build lasting partnerships that lead to smarter innovations for our customers. These customer stories demonstrate our commitment and success in providing customers like you with improved power solutions through world-class innovation in a number of industries.

Filter Case Studies

Poland’s impressive history in maritime research will continue to grow with the delivery of two new multipurpose vessels in the second and third quarters of 2020.  Under construction at the noted Remontowa Shipbuiding yard in Gdańsk the two 60 by 12.8-meter vessels will replace two 35-year old vessels working under the direction of the maritime office in Szczecin and Gdynia. The diesel

The Zhoushan Islands are just off shore of east China's Zhejiang province, and lie south of Shanghai on Hangzhou Bay. The main island is home to a naval base, shipyards and a port. It is a busy island with a well-developed ferry system carrying both people and vehicles back and forth to the mainland. A fine new 690-passenger ferry, Zhoushan Islands Prosperity, has recently been added to this fl

With a rugged coastline and many fjords to cross Norway has become a world leader in progressive ferry design. Turkey, with a skilled work force and broad marine experience has become a leader in ferry construction. Put the two together and you have the teamwork that results in the Basto series of RO-RO ferries. The latest in the class, Basto VII, to be launched in December of 2019, will be pow

Preserving the natural environment is a responsibility railroads are taking seriously. Although all rail industries are pushing for this, freight has less pressure to push for cleaner, which is why it is extremely noteworthy that Cummins Rail and R.J. Corman Railpower partnered in creating a locomotive that meets Tier 4 Final emission standards.  Cummins Rail Segment stands on the company’s p

In February of 2018, a coal mine in Northwest Colorado purchased a Liebherr R 9400 excavator for use at its mining operation. The coal that is unearthed at this site is delivered directly to an adjoining 885 megawatt, coal-fired power station. Mine sites in extreme environments require dependable engines to power their mining applications, which is why this mine called on Cummins to power their Li

When it comes to selecting a design for a new series of vessels, the most important consideration is to recognize the craft’s purpose and develop a form to meet that function. Cooke Aquaculture in Atlantic Canada has a number of fish farms located in protected waters around the Maritime Provinces. Supplies and gear have to be transported between the farms and the shore. To meet this demand they

The export of refined iron ore from Australia to China has led to the development of gigantic infrastructure especially for the loading process from shore to ship. The company web page describes this process as follows: “The magnetite concentrate is exported to China from a purpose-built port at Cape Preston. From the stockyard, the product is transported to the barge loading berth at the break

To be an accomplished diving master in Thailand with access to both the Andaman Sea and the Gulf of Thailand would be about as good as it gets. But it is one huge step up the joy register to own your own diving support vessel. This is especially true if you can also accommodate 30 fellow divers and a supportive crew of eight to cater to the divers’ needs and navigate the vessel. That will be

Cummins provides more than just engines to serve its fleet of engines at the Julong Mine. The most valuable mineral resources are usually excavated in hard-to-reach locations around the world. This causes difficulty not only for the miners, but also for the heavy machinery used at mine sites. Some of these mines operate at high altitude, where the air quality and severe weather conditions can c

From the early 17th to the mid 18th century the Dutch maintained a post on the Chao Phraya River near the ancient Thai capital of Ayutthaya. Today little remains of the old Dutch buildings but a fine new museum has been built on the site, Baan Hollanda informs the modern visitor of that important era. Next door to the museum a living and working record of the proud history of Thai boat building

A recent report by the Ghana Ports and Harbour Authority states, “Total cargo traffic for both ports (Tema and Takoradi) grew from 19,459,834 tonnes in 2016 to 22,086,626 tonnes in 2017, registering a 13 per cent increase. Transit cargo in both ports also increased from 944,081 tonnes in 2016 to 1,249,336 tonnes in 2017, a rise of 32 per cent. Container traffic for both ports rose from 942,463 TEU

Fish companies from New Zealand to Russia (currently 24 large and ultra large Russian vessels) and Iceland to the USA as well as Greenland and now Canada have chosen the Norwegian firm Skipsteknisk when it comes time to design a new vessel. The firm has garnered a reputation for designing and overseeing the construction of vessels that integrate the most up to date technology from deck equipment t

According to Wikipedia, “Indonesia has a total land area of 1,904,569 square kilometres (735,358 sq mi), Including 93,000 square kilometres (35,908 sq mi) of inland seas (straits, bays, and other bodies of water). The additional surrounding sea areas bring Indonesia's generally recognized territory (land and sea) to about 5 million km2.” The nation of over 17,000 islands has 54,720 km (34,000 m

In September 2018, a 17-by-5 meter catamaran completed its final tests in the Tigre Delta of the Tigre on the Parana River near Buenos Aires, Argentina prior to its delivery to her Chilean owners. The cat was designed by Eng. Emilio Noel and built by Astilleros Unidelta SA. which has a well-established reputation in a wide range of steel and aluminum workboats. The yard has a plant located in B

Paraguay’s Tsuneishi Shipyard, a subsidiary of the Japanese firm of the same name, recently delivered the powerful towboat Tebicuary 3 to her owners Navegación del Sur S.A. (Navesur) in June of 2018. The new vessel is a near sister-ship to the 2015-delivered Ceasar Primo for a different owner. The newer vessel will also work on the Paraguay-Paraná River system that provides marine access to lar

Cummins Vessel Reference #836 Wise visitors to Bangkok will be sure to take a Chao Phraya river cruise past the spectacular Temple of the Dawn, Wat Arun, and the glories of the golden spired Grand Palace. The ultimate way to do this is on a dinner cruise with a buffet of the celebrated Thai food. This has become such a popular experience that the river at night becomes a spectacular para

Cummins Vessel Reference #832   After 60,000 hours of service, crab fisherman Robert Ross decided that his 19-liter Cummins 1150M had earned a rest. The 500 HP engine had been a perfect match for his 72 by 26-foot aluminum boat so he ordered up a new Cummins KTA19-M3 at 500 HP, continuous duty, from his local supplier Cummins Sales and Service in Fredericton, New Brunswick, in easte

Cummins Vessel Reference #830 The Island of Zanzibar and others in the group are located just off the coast of Tanzania and have, for thousands of years, been a destination for adventure, beauty and trade. The earliest Arab traders brought the skills of dhow building and, along with this, a great appreciation of quality boats. While dhows are still built in Zanzibar, the owners of Azam Mar