Cummins Case Studies

We’re in it for the long haul. We build lasting partnerships that lead to smarter innovations for our customers. These customer stories demonstrate our commitment and success in providing customers like you with improved power solutions through world-class innovation in a number of industries.

Filter Case Studies

Cummins Vessel Reference #732 The Captain D: all dressed up and ready to go. Established in 1928 by George Lyon Sr, Lyon Shipyard today occupies 30 acres of waterfront near downtown Norfolk Virginia. Norfolk Tug is based in the same area and takes pride in operating a fleet of tugs from the 1970s and ‘80s that they proudly designate as “vintage steel”. They also have an aggressive program of

Cummins Vessel Reference #727 A recently launched trawler is fitting out alongside at Mahachai Dockyard. After a bit of a lull in construction, the Mahachai Dockyard had six trawlers in various stages of completion in mid-April of 2014. Ranging in size from three 45-meter, one 38.5-meter and two 25-meter vessels all six will be powered by Cummins KTA38 engines generating 800 or 1000 HP dependin

Cummins Vessel Reference #730 The Erin C Grenon on the Mississippi River.   Over the past decade Blessey Marine has taken delivery of a large number of Cummins-powered pushboats for their inland fleet. The vessels are sized to share a common versatility with the draft and horsepower to work both the shallower waters of the Intracoastal Waterway and power for the big flows of the

Cummins Vessel Reference #729 S.P. Inter Marine crane barges off loading a cargo ship. Long established in the trucking, warehousing, cargo transfer and barging industry of Thailand, S.P. Inter Marine can be described as a broadly horizontally integrated firm. But established success doesn’t mean they are sitting still. With an well constructed presence at Ayutthaya, about 80 kilometers up the

Cummins Vessel Reference #725 The Sea Cypress completing sea trials.   Over the years, Rodriguez Shipbuilding Inc, of Bayou LaBatre Alabama has probably delivered more shallow-draft tugs than any other US-yard. Their signature lugger-type tug design, with its distinctive aft cabin and wheelhouse, has a strong following amongst US Gulf Coast operators servicing near shore petro-op

Cummins Vessel Reference #726 left to right: Sakchai Rujiphapra, Director, Mahachai Dockyard; Sathit Suwanprasert, Senior Engineer, Marketing Dept., Cummins DKSH (Thailand) and Ku Wee Ming, Manager, Regional Marketing, Cummins Asia Pacific with the newly launched Wonderful Pearl currently being fitted out alongside at the shipyard.   Thailand has long been noted for exquisite fo

Cummins Vessel Reference #724 The Bravante V on sea trials. Long reserved for specialized applications such as icebreakers, diesel electric has enjoyed a rapid growth for marine propulsion in the past decade. Throughout that period, Cummins Marine has been a leader, supplying over 900 diesel electric packages since delivering its first genset 2003. A QSK60 genset ready to delivery from Cu

Cummins Vessel Reference #722 Mr. Ernie: A New Generation in the GOM. The latest delivery from Houma, Louisiana-based New Generation Shipbuilding is representative of the New Generation in supply vessel design. The distinctive bow and focsle profile on the 171 by 36-foot Mr. Ernie is reminiscent of some of the progressive International designs. This can be attributed to additional super structu

Cummins Vessel Reference #720 One of the first steel-hulled crewboats being loaded out in Vietnam. Australia-based Strategic Marine bas built a strong reputation for high performance crew boats. Primarily built at their Singapore shipyard, the aluminum crewboats are available in a variety of sizes and power configurations. In recent years, Strategic has delivered a number of their popular 40

Cummins Vessel Reference #721 The diesel-electric tuna seiner Belle Isle.   As the ex-vessel cost of tuna continues to squeeze the margins for tuna canners, the advantages of high quality and high value sashimi grade tuna become ever more attractive. Writing for their April 2013 in-house publication, SAPMER CEO Yannick Lauri explained the French firm’s Indian Ocean tuna fishery,

Cummins Vessel Reference #719 The 1400 cubic meter capacity LPG tanker ready for delivery. The Saigon Shipbuilding & Marine Industries One Member Co, Ltd. (Saigon Shipmarin) has completed construction of a 60 by 11-meter LPG carrier. With capacity for 1400 cubic meters in two tanks the vessel’s hull has a 4-meter molded depth and a 2.6-meter draft. Designed by a related company to Saigon

Cummins Vessel Reference #717 Harley Marine's new push boat Stardust ready to leave the yard.   The maritime community in the United States has watched with interest as Harley Marine Services has expanded from the West Coast, to the East Coast, the Gulf Coast and now the Inland Waterways. As with other expansions, carried out by Chairman and CEO Harley Franco, this one, the tent

Cummins Vessel Reference #718 The Cargotec gen-set package. While the larger and faster container ships and their shore-side cranes have been getting much of the press of late, there remains a huge volume of bulk cargo shipping. A long established manner of handling bulk cargos has been to move them by crane from a deep-sea ship to inland or coastal barges. This can be done directly, with the

Cummins Vessel Reference #716 MV Gunner on the Intracoastal Waterway.   In mid-October of 2013 Capt. Mark Duthu of Montgeut, Louisiana was proudly showing his family around his new command. The 72 by 30-foot pushboat MV Gunner was about to leave the New Generation Marine Shipbuilding on the Intracoastal Waterway near Houma Louisiana. With the Louisiana Marine Operators logo prou

Cummins Vessel Reference #713 A rendering of Q-West's current build project. As with most island nations, New Zealand is heavily dependent on ferries. By this time next year, there will be a new ferry added to the Auckland-based Fullers Group fleet. Currently being constructed at Q-West Boat Builders Ltd. on the Wanganui River, the Incat Crowther-designed catamaran will join a large number of

Cummins Vessel Reference #678 On the Rio Negro at Manaus.   A thousand miles (1600 Kilometers) up the Amazon River the Port of Manaus has long attracted ocean going vessels. In the 19th Century they came for rubber, today the products are more varied with a duty-free zone generating additional commerce. Other ports along the Amazon may be for a single commodity such as soyabeans

Cummins Vessel Reference #707 Ready for Work It is said that only about 2000 of the Philippine’s 7000 plus islands are inhabited. But that is a very large “only”. It is doubtful if any other country has greater need for ferries. A visit to the port of Cebu, with ferries ranging from out-rigger-fitted wooden boats (Bangka) to large steel cargo ferries crowding the harbor, shows just how varied i

Cummins Vessel Reference #706 The Mainport Cedar ready for work.   On their web site, Mainport says, “All business is about interaction between people”. The firm, based in Cork Ireland, has demonstrated this throughout their business. These include a range of subsidiaries in diverse marine fields and diverse locations from South Africa to the Caspian and at home in Ireland. &