Greek Ferry: Four Legs for Power | Cummins Inc.
""
Marine

Greek Ferry: Four Legs for Power

by Alan Haig-Brown

Cummins Vessel Reference #608


In the near future some marine passengers in Greece will be driving their cars aboard a handy size and handy maneuvering double-ender car ferry. The 88 by 17.6-meter vessel is undergoing final fitting out at the Sidironaftiki Epe-Atsalakis shipyard in Piraeus. The owners, Agios Athanasios A Shipping had the vessel designed by naval architect Nikos Petichakis.

Capacities include 130 cars on the main deck and 36 cars on a lower deck as well as 500 passengers. Tankage for fuel includes 65 tons with a 10-ton day tank in addition to 120 tons of water.

Propulsion for the ferry, named Panagiotis D, includes four Veth Z-Drive 400 (RR 4.1/1) drive “legs”. Each leg is powered by a Cummins KTA19-M3 engine generating 600 BHP at 1800 RPM. The four Z-drives, mounted one in each corner of the vessel, carry 1250 m/m propellers for a design speed just over 14 knots.


For further information:

Mr. Spyros Athanasioy
Agios Athanasios A Shipping
Greece
Phone: 302 1046 51006

Sidironaftiki Epe-Atsalakis
38 Dimokratias Ave Str
Perama Pireaus, Greece
Phone: +302 1044 15921
Nikos Petichakis
Naval Architect
Sotiros 13-15
Pireaus
Phone: 302 1041 78152

Antonis Petridis
Sales Engineer Marine Engines
ERGOTRAK SA
Phone: 210 629 3482
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...