Re-Thinking the Re-Power | Cummins Inc.
""
Marine

Re-Thinking the Re-Power

by Alan Haig-Brown

Cummins Vessel Reference #694

The DD Catherwood was designed with the option of a side installation of new engines.

 

When the opportunity arose for Ernie Catherwood to add a good tug to his 14-boat fleet at Catherwood Towing, he did the math and took the deal. Catherwood Towing has grown up around log towing in the Fraser River. The work, known as “yarding” generally employs boats in the 25 to 43-foot range. Catherwood has several of these boats, most powered by twin Cummins KTA19 engines.

 

To diversify their operations Catherwood has been doing more barge work and now has contracts to tow gravel from a quarry about 30 nautical miles north of the Fraser River. They have also picked up a couple of freight runs towing barges with truck trailers. To better serve these contracts the company has purchased some larger “outside boats” as the opportunity arises. Such was the case when an owner of a 74 by 25-foot boat phoned Ernie to see if he was interested in adding to his fleet.

 

 

A sliding “barn door” allows the boat to be locked up when the crews are not working but gives quick access during the day.

 

The 39-year old boat was at a shipyard undergoing a scheduled Canadian Steamship Inspection. Ernie had marine surveyor Mark McAllister and his port engineer Trevor Sexton check the boat out. They reported the boat sound with excellent 1/2-inch hull plating. But the old 12V149 Jimmies were tired, although their big Lufkin gears had recently been rebuilt and were in good shape.

 

Ernie decided that if he could repower the boat with a new set of Cummins KTA38 engines at the right price he could make some money with the tug. Todd Braconnier of TCB Marine Consulting proposed that they use a well-proven process of installing the new engines through the side of the hull rather than the traditional lowering in from above and moving forward into the engine room. Mark McAlister explained that design forethought by the builder in placement of tanks and auxiliary machinery on the tug made this method much simpler.

 

 

The port engine in place in the tug DD Catherwood

 

We were able to do the engine swap with this method for half the cost of stripping the engine and going in from the hatch in the aft deck,” Catherwood said, “The savings in labour with workers not climbing up and down to the main deck are significant but more importantly the crew at Arrow Marine terminals, where we are doing the job, were able to remove the old and set the new engines in place with a fork lift. With long forks, even the starboard engine, opposite the hull opening, could be set.

 

 

 

When all is done the tug will have a spacious engine room.

 

The engines were coupled to the existing air-controlled Lufkin gears that are each nearly the size of the engines. In addition to air-clutches the gears have air-controlled shaft brakes. The 7:1 reduction allowed Catherwood to keep the big 84-inch 3-blade props that turn in kort nozzles.

 

 

 

Ernie Catherwood grows his fleet through careful planning.

 

In addition to the main engine repower Catherwood has installed two new 50 kW gen sets, upgrades to the electronics included 40 wheelhouse-alarm sensors for the engine room, complete overhaul of the Burrard towing winch and rebuild of various components and piping. The winch is fitted with an air-controlled brake and carries 2400 feet of 1.25-inch wire. For Canadian manning and regulatory reasons, Catherwood will set the new engines for only 500 HP each, but the bigger boat, renamed DD Catherwood, with its powerful gear-prop combination will do much to assure “just-in-time” delivery on the company’s chartered freight runs regardless of weather conditions.

 

 

All photo courtesy of Haig-Brown/Cummins

 

 

For further information:

 

Ernie Catherwood
Owner, Catherwood Towing Ltd,
101-32885 Mission Way,
Mission, BC
Canada, V2V 6E4
Phone: 604 462 9221
E-mail: [email protected]
Web: http://catherwoodtowing.com

Mark McAllister
McAllister Marine Survey & Design Ltd.
8466 Cox Dr.,
Mission, BC
V2V 6V3
Phone: 604 209 8847
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...