Philippine Fleet Builds for Reliability | Cummins Inc.
""
Marine

Philippine Fleet Builds for Reliability

by Alan Haig-Brown

Cummins Vessel Reference #667

The M/T Jewel Faith nearing completion.

Earlier this year, Swordfish Marine of the Philippines, launched a new coastal tanker the M/T Jewel Faith. The new vessel is 69 meters in length with a 12.8-meter beam and a 2.8-meter draft.


Looking forward over the main deck of the tanker.

To assure reliable propulsion on a vessel carrying petroleum products the owners chose a pair of dependable six cylinder Cummins KTA19-M3 engines. Delivering a total of 1200 hp through ZFW650 gears with 5:1 reduction to a pair of 1574 m/m propellers, they give the tanker a speed of ten knots.

The Jewel Faith was built by and launched from the Josefa Slipways in Navotas City.


Photos courtesy of Cummins Sales & Service Philippines, Inc.

For further information:

E.P. Crisostomo
Swordfish Marine Services Corp.
70 Tenth Ave., West Grace Park
Caloocan City, Metro Manila
Philippines
Phone: 63917 829 2938

Josefa Slipways Inc.
1326 M. Naval St.,
San Roque,
Navotas City
Philippines
Phone: 632 2837586 | 632 2838488
Web: http://josefaslipways.com/

Antonio M. Corona, Jr
ESG Application Engineer or Aris T. Articulo
ESG Sales Staff
Cummins Sales and Service Philippines Inc.
Lots 1&2, Block 15, LIIP Avenue,
Laguna International Industrial Park, Mamplasan,
Binan, Laguna 4024
Philippines
Phone: 02 717 8100
Cell: 63917 527 3137
Fax: 6328430703
Web: cummins.com
Email: [email protected] | [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...