Hydrogen | Cummins Inc.
for-a-world-thats-always-on_dupe32
Start your shift to cleaner power

At Cummins, we understand the importance of following regulations while meeting business needs. As regulations evolve, we’re here to help you navigate the energy transition and innovate towards a future of smarter, cleaner power.

Hydrogen technology by Cummins

By investing in innovative hydrogen solutions, we’re paving the road to clean power that helps you meet regulations, reduce emissions, and futureproof your business.

Hydrogen Engine

Hydrogen engines

Hydrogen internal combustion engines produce zero emissions and can help reduce greenhouse gas emissions.
Accelera powered truck

Fuel cell technology

Zero-emissions technologies like fuel cells have the potential to decarbonize the world’s hardest-working industries.
senior-technician-working-on-an-accelera-zero-emission-truck.jpg

Electrolyzer technology

Electrolysis is a highly efficient electrochemical process used to convert water into hydrogen.

Why hydrogen fuel is the future of clean energy

As one of the most abundant elements in the universe, hydrogen is an essential part of how companies can meet their decarbonization goals and reduce their environmental impact.

No direct CO2 emissions

Hydrogen power reduces greenhouse gas emissions through fuel cells, which convert hydrogen to electricity, to power vehicles while releasing nearly trace amounts of carbon dioxide.

Renewable and readily available

Hydrogen is a renewable source that can be readily produced from water using renewable electricity. It burns without emitting greenhouse gases.

Long-term storage

Storing hydrogen onboard motor vehicles is safe, and with a storage pressure of 700bar, it enables more onboard fuel storage and an extended range.

Quick refueling capabilities

Hydrogen engines offer quick refueling times and diesel-like performance, durability, and reliability. Unlike electric vehicles, hydrogen vehicles do not need extra time to charge.

FAQs about hydrogen gas fuel

Hydrogen fuel cells generate electricity through an electrochemical reaction where hydrogen and oxygen combine to produce electricity, water, and heat. They power vehicles using hydrogen, a zero-carbon fuel, by supplying electricity to an electric motor. Fuel cell hydrogen vehicles (FCEVs) are efficient for lower loads or operating without a load.

Read More

Hydrogen is easily produced from water using renewable electricity through a process called electrolysis. In this highly efficient electrochemical reaction that takes place in our electrolyzer system, water converts into hydrogen and generates hydrogen gas. This process emits no greenhouse gases and is both colorless and odorless.

Read More

Green hydrogen is produced using renewable energy sources like solar, wind, and hydropower to electrolyze water. The resulting reaction produces only hydrogen and oxygen, meaning the process doesn’t emit any carbon dioxide. Green hydrogen is the only color in the hydrogen rainbow that produces zero harmful greenhouse gas emissions.

Read More

Hydrogen engines are internal combustion engines that burn hydrogen as fuel. They are as reliable and durable as diesel engines and have many of the same components such as an engine block, crank, and installation parts. Hydrogen engines also look, sound, and work like internal combustion engines.

Read More

Hydrogen can be delivered or produced on-site. A hydrogen fueling station allows vehicles using a gaseous or liquid delivery model to refuel. Unlike electric vehicles, which can take a long time to fuel, hydrogen engines offer quick refueling times and diesel-like performance, durability, and reliability.

Read More

Connect with us