How do fuel injectors work? | Cummins Inc.

How do fuel injectors work?

By Cummins Components Business Unit

Fuel injector generating power.

The best fuel injectors enable an engine to generate maximum power while minimizing fuel consumption and reducing pollution. Fuel injectors with the latest technology help reduce carbon and greenhouse gas emissions by delivering accurate fueling with optimized air mixing. This article outlines what a fuel injector is and how it works in diesel, natural gas, and hydrogen engines as well as in hydrogen fuel cell vehicles.

Infographic card
Click the image to open a hi-res version of this infographic in a new window or tab

What does a fuel injector do? 

A fuel injector regulates the injection of fuel into an engine’s internal combustion chamber where it is mixed with air and ignited. The combustion chamber is where the chemical energy in diesel, hydrogen, and natural gas is converted into power for the vehicle. When actuated by the electronic control unit (ECU), the injector delivers a precise amount of fuel to ensure efficient combustion.

How does a diesel injector work? 

A fuel injector in a diesel engine consists of a solenoid (a type of electromagnet), a nozzle, and a needle within the injector body. Modern diesel engines are direct injection, meaning fuel is delivered directly into the combustion chamber.  

In the cylinder, air is compressed by the upward movement of the piston. As the piston nears the top of its path, an electrical signal is sent to the solenoid, causing the injector needle to lift, and allowing high pressure fuel (up to 37,000 psi) to flow through the nozzle and into the combustion chamber to mix with air. Because of the elevated temperature created by the compression stroke, the air-fuel mixture auto-ignites, creating power and driving the engine's pistons.  

The combination of high fuel pressure and exceptionally fine injector nozzle holes ensures optimal mixing of air and fuel to meet even stricter emissions standards. In diesel engines, a fuel injector can fire multiple pulses in a single power stroke which can be used for noise mitigation and emissions control.

How does a natural gas injector work? 

Natural gas engines function similarly to gasoline engines in that their combustion process utilizes a spark plug (unlike diesel engines). Natural gas is compressed and stored in a fuel tank, typically located in the back of the vehicle. The high-pressure gas is routed through a pressure regulator that reduces the pressure of the incoming fuel to an appropriate level to ensure accurate fueling from the injector. An electrical signal opens the injector and ensures the correct volume of fuel is delivered into the intake air stream. That air-fuel mixture is delivered to the combustion chamber where it is ignited by the spark plug, creating power.

Natural gas is a lower carbon-intensity fuel compared to diesel and is considered a critical technology to help fleets reduce carbon emissions today. Natural gas can be leveraged for immediate reduction, and, in the case of Renewable Natural Gas (RNG), it can even possess negative carbon-intensity 

How does a hydrogen ICE injector work? 

Hydrogen engines have a high degree of components common with natural gas and diesel engines. Cummins’ hydrogen engines are built on the cutting-edge fuel agnostic engine platform. Though they share common components, hydrogen engines have specific requirements for regulating and injecting fuel. This is because hydrogen is more flammable than diesel and is easier to ignite in a combustion chamber. Because of this, hydrogen engines can have “pre-ignition” issues, which may cause backfiring. One way to overcome pre-ignition issues is for an engine to use a direct injection system. Direct injection systems introduce hydrogen directly into the cylinders. Cummins is currently developing a 15-liter hydrogen engine that uses direct injection. 

What is the injector system in fuel cell vehicles? 

Hydrogen fuel cell vehicles harness electrical energy produced by splitting a hydrogen atom into protons and electrons and reacting it with oxygen.  On fuel cells, the hydrogen delivery system must provide sufficient fresh flow of hydrogen to the anode side of the fuel cell stack to meet the electrical power demands of the application. This can be accomplished using either a hydrogen injector or proportional valve, both of which accurately regulate the flow of hydrogen to the stack. Unlike diesel, natural gas, and hydrogen internal combustion engines (ICE), fuel cells do not have any carbon or pollutant emissions. The byproducts of splitting a hydrogen atom in a fuel cell are electricity, heat, and water vapor. 

What is the role of fuel injectors in energy transition? 

Fuel injectors are more than just a component in engines. They can play a key role in the energy transition from fossil fuels to cleaner energy sources. By optimizing fuel consumption in traditional diesel engines and facilitating the operation of alternative fuel engines like natural gas, hydrogen internal combustion engines (ICE), and hydrogen fuel cells, fuel injectors contribute to trucking fleets’ efforts to reduce carbon and greenhouse gas emissions.  

Read more about Cummins fuel system products. Cummins stands ready to partner with on-highway and off-highway vehicle fleets to help them get the most out of their engines while achieving sustainability goals. Contact your local Cummins sales office today to learn more.  

Accelera™ by Cummins works on the development of new technologies in fuel cells. Accelera, a business segment of Cummins, is both a components supplier and integrator, focused on batteries, hydrogen fuel cells, e-axles, traction drive and electrolyzers. For more information on the diverse Accelera portfolio of zero-emission solutions please visit accelerazero.com.

Request a quote

Author Profiles

Cummins Components Business Unit

Components Business Unit