Fixed-mount installed RV generators | Cummins Inc.

Get more out of your RV adventure with an installed Cummins RV Generator

Consistent Power

Cummins fixed-mount RV generators give you reliable, consistent power, just like home. Run your RV's AC, TV, fridge and lights and have all the electricity you need.

Freedom to go anywhere

There are no more limits now that you can take your RV anywhere. You have the power you need and the freedom to go wherever, whenever. Our vast support network is never far away.

Restored Vacation Time

The many tasks you do to get your RV ready for your camping trip just got easier. Keep your next adventure simple and spend more time with family and friends with an installed generator.
Family sitting outside RV in driveway

Don't miss out on your vacation because of these common issues

Make the most of your vacation with a fixed-mount RV generator
  • Lost power - Your generator runs out of gas or fails when too many appliances are running, disrupting your relaxing vacation.
  • Lost vacation and family time - Setting up a portable generator can be complicated and time consuming. It also takes up precious RV space along with the cans of gas it requires.
  • Disrupted peace - Generators that are fixed-mounted in your RV are enclosed and quieter than other power sources so you can enjoy the peace and quiet.
Truck driving up a mountain in the desert

Convenience is key

How to decide between an installed or portable RV generator

Will an installed generator really improve your RV experience? Convenience is a key feature.

  • The investment in an installed generator is worth it for many owners thanks to the protection that comes with installation. The generator itself is protected from the elements, fixed in its own compartment. It's secure, too - it will be bolted into your RV for stability and security wherever you roam.
     
  • Installed generators save you the hassle of moving the generator in and out as you change locations. Since it won't need gas cans or extension cords, you save precious space and setup time.
     
  • If a fixed-mount generator is right for you, let us connect you with an authorized dealer who will schedule your installation and guide you through the process.
     
  • With your newly-installed RV generator, you'll be able to explore the farthest destinations with ease, from the comfort of your home on wheels.
rv parked on dirt road in desert

Sign up to receive RV updates

Want to be kept in the loop on what’s new from Cummins?

Subscribe to our email list and receive messages (not more than two per month) that will provide new product updates as well as reminders and RVing tips and tricks.

Onan RV Generators

Units

Frequency (Hz)

60

Fuel Type

Diesel

13 - 25 of 13

We have your power covered

100 +

years powering the world

3 M+

RV generators sold

600 +

service centers in North America

Chase Briscoe's Cummins RV Generator Experience

 

 

Ready to power your RV with a fixed-mount generator?

 

Buy now

Woman drinking coffee outside her RV looking at a mountain
Frequently asked questions about fixed-mount RV generators

A fixed-mount generator in your RV means that you won't have to drag out a portable generator for your morning coffee. Installed generators make life easier on the road - and less complication means more fun.

That’s the beauty of a fixed-mount Cummins generator. Simply hit the switch and enjoy your cup of coffee. Turn it off, and you’re ready to hit the road.

Not only do you save time and effort so you can enjoy your vacation, but there are other perks to investing in a fixed-mount generator for your RV.

Here are answers to some common questions about installing a generator in your RV:

FAQs

Yes. You have the freedom to run all your appliances at once if you wish. No more choosing what gets power or taking turns with appliances.

Yes. Fixed-mount generators can last over 10 years, are securely installed in your RV, and are better protected from weather and theft, making them a great long-term investment with great value over other options.

The last thing you want when you’re out enjoying nature is the sound of a chugging generator in the background. You want to enjoy the peace and quiet on your vacation. We help you keep it as quiet as possible with our fixed-mount generators registering as low as 65 decibels (at 10', half load). That’s the equivalent of soft background music or normal conversation.

With over 600 Cummins Sales and Service locations in North America, we are here for you wherever you go.

Yes. Campgrounds are sometimes booked out in advance, so you have to make your own campsite. But don’t let that hinder your RV experience. With an Onan generator, you have the power to go wherever, whenever.

We're ready to power your RV adventures

 

With an installed RV generator, you'll be able to focus on your trip and the memories you’re making instead of worrying about the tasks involved with other power sources. Imagine a peaceful, uninterrupted RV adventure where you have the power you need, when you need it. We'll take care of the power so you can sit back, relax, and enjoy the journey.

Connect with us