Philippine Landing Craft | Cummins Inc.
""
Marine

Philippine Landing Craft

by Alan Haig-Brown

Cummins Vessel Reference #671

The landing craft Sir Carlo.

The province of Surigao del Sur is located on the northeast corner of the Island of Mindano in the Philippines. The locally owned CTP Construction and Mining Corporation operates a nickel ore mine there and has recently taken delivery of a new landing craft. The 70.59 by 14.6-meter vessel was designed by naval architect Edward Cruz of Baseco, Tondo Metro Manila. Built by Sea Rudder Incorporated, also of Baseco, Tondo, the landing craft is named Sir Carlo.

Main engines of the landing craft are a pair of six-cylinder Cummins KTA19-M3 diesels each producing 600 hp at 1800 RPM. The engines turn 1727 m/m propellers through ZF W650 gears with 5:1 reduction. This gives the vessel, with its three-meter draft, a speed of ten knots.


For further information:

Aris T. Articulo
ESG Sales Staff
Cummins Sales and Service Philippines Inc.
Lots 1&2, Block 15, LIIP Avenue
Laguna International Industrial Park, Mamplasan,
Binan, Laguna 4024
Philippines
Phone: 02 717 8100
Cell: 63917 591 5306
Fax: 6328 430703
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...