Cummins Vessel References | Cummins Inc.

Cummins Marine Case Studies

Shipbuilders and sailors all over the world depend on Cummins engines and generators to power their vessels. Whether you're on the water for fun, profit, or adventure (or all three), you know that Cummins has you covered.

Esteemed marine authors Alan Haig-Brown and Lisa Overing write the interesting and insightful vessel references listed below, complete with contact information if you want to know more about each installation.

Blue and white boat

Filter Case Studies

Enforcing the law doesn’t just happen on land; it is also essential at sea. With record interdiction using tough, lightweight aluminum patrol boats, the success of the National Security Cutter program at apprehending criminals is remarkable. The 11M Long Range Interceptor II is just such a vessel, designed to pursue high-speed target craft for vessel board and seizure, rescue, and recovery. Eng

With the regulated catch quotas of contemporary fisheries, design versatility for a fishing boat can be important. A new 19.81 by 7.31-meter (65X24-foot) combination crab trap and groundfish trawler designed by NAVANEX for building by Chantier Naval Forillon, both of Gaspé, Quebec, Canada is a fine example of this. Owners, Listuguj Mi’gmaq Government, anticipate accepting delivery in April of 2022

With excellent fuel economy for long-range cruising coupled with dependability and endurance proven through thousands of hours of reliable commercial and trawler operation, the new Cheoy Lee 107 explorer yacht is powered by twin Cummins QSL9’s. Expected for delivery in 2022, this long-range cruising yacht is a fuel-miser capable of voyaging anywhere in the world. The 107 is an expedition vessel

With the most prolific big game fishing on the planet, Costa Rica is a stunning destination for the avid angler. During peak season, the best sportfishing boats in the world migrate to Costa Rica’s Los Sueños South America Puntarenas. Whiskey Blues stands out in the fleet. This 2008 47 Convertible Maximus American Marine Boatworks sportfishing classic was a custom one-off created by hardcore fishe

“Builders choose Onan generators because of the ease of using Onan, and it is backed by Cummins, so the supply chain should be better, too." Fishermen appreciate quiet Onan gensets Custom-built pleasure crafts represent the ultimate vessel in luxury design, naval architecture and craftsmanship. As the epitome and vision of a discriminating, private yacht owner, one-off dreamboats demand pr

"I’m a big believer in Cummins products, and I’ve never had a problem getting Cummins parts." — Capt. Norm Bekoff Do the math: Counting on Cummins cuts fuel costs in half! Several variables impact the success of a commercial fisherman with a charter operation. There’s the unpredictable weather, identifying a hot fishing spot and getting potential customers to choose your boat – it’s a com

License to Thrill Always moments away from leaping aboard a classy powerboat and then driving it like he stole it, the fictional James Bond would gravitate to the Technohull Omega 47 for his next dramatic, implausibly long, high-speed boat chase from some nefarious villain headquartered in a remote island compound. The Technohull Omega 47 luxury RIB is a Bond-inspired, high-performance speed

"The Cummins KTA19s provide the perfect amount of power to do our job." — Brennan Templet, mate and pilot of Richard B Scream all you want in the swamp, no one will ever hear you - or help you. Down on the bayou, autonomy and self-preservation is key, because in a remote area, you’re on your own, in the elements. Having an engine like the Cummins KTA19 with torque, power and maneuverabi

"Up here, near Cape Cod, there’s a lot of support [from Cummins]. The Dunham dealership is open all the time. I also have Cummins X15’s in all my work and pickup trucks for my excavation company." — Capt. Anthony Belculfine  Smart diesel QSC8.3 600 gets out in front of the fleet The shocking combination of horsepower with efficiency is just one benefit of finding the perfect boat and

Liveaboard, Spanish-inspired llaut loaded with style, creature comforts Wrapped in luxury amid the waves gently lapping the hull of the Menorquin 68 is a sensual experience at sea. Three lovely staterooms with four berths encourage sleeping in just a little bit longer. Upon awakening, stepping up the companionway into the well-appointed salon's open entryway brings the sunlight in with the sea

“The whisper-quiet genset, proven reliability, ease of maintenance and longevity are prime reasons why Nordhavn’s long range vessels are built standard with Onan marine generators.” - Jim Leishman, Vice President & Co-owner, Nordhavn Yachts Nordhavn 41 fuel-miser boasts a small carbon footprint The Nordhavn 40 set the world record for a production boat under 70 feet, circumnaviga

Modutech Marine, of Tacoma, Washington, has gained recognition on meeting the stringent conditions of military contracts. In 2020 they completed a contract to build a fleet of five small tugs. These carry the military designation Work Boat Docking.   Compact and highly versatile Modutech’s Brian Swindahl describes the vessels, “The mission of the CNIC Work Boat Docking (WB Docking) i

“We can confidently say that this project will be a real revolution in the towage operations and a great milestone for our green tug solutions." - Noyan Altuğ, CEO of UZMAR The concept of ‘hybrid tug’ is getting a whole new definition with an innovative new tug under construction at Turkey’s Uzmar Shipyard for the Danish Port of Aarhus. From the outside it looks very similar to other Robert

“Loaded with creature comforts, the audio in an Azimut is like a night club with an amazing sound system.” - Peter Kurki, Sales Executive, Allied Marine   Semi-displacement hull for smooth sailing in Azimut style Azimut, the world’s leading builder of seductive, fast-planing flybridge yachts, now builds vessels for long-range cruising. The 43 navetta-style yacht is the fourth m

As progressive nations worldwide commit to reducing greenhouse gases, a fishing vessel is built to do its share with Cummins marine propulsion. Designed by Norway’s Skipsteknisk and Selvåg AS, the Selvåg Senior is under construction at Cemre Shipyard for Sorheim Holding and is truly a remarkable concept. Capable of both trawling and purse seining, the 79.5 by 16.2-meter vessel with have a molde

Voyage confidently in the Fleming 55, the ultimate passagemaker Open oceans. Icy fjords. Inland rivers. Tropical seas. Aleutian Islands. Florida Straits. Designed for serious cruising in every condition, the Fleming 55 is a raised pilothouse motoryacht for a capable owner-operator voyaging the world in confidence and comfort.  The Fleming low profile provides stability and comfort at se

“The QSB6.7's are tried, true and exceptionally reliable. There is extra strain on a high-speed vessel... That’s why we use Cummins. Their marination is simply better.” - Nick Williams of SMJB Thrills and water adventures Smoking hot! Powered by twin 350HP Cummins QSB6.7’s with 274 Hamilton Jets, this Subchapter-T passenger vessel for Miami WaterSports is built to fly, spinning exc

Custom built for offshore tournaments With large cockpits and custom configurations, Henriques Yachts produces canyon-capable fishing machines with the muscle and seakeeping capability of a real, rough-water boat.  Capable of venturing out safely in the chop over 100 miles to reel in a big trophy tournament fish, the strong and solid Henriques hull is strategically designed to endure ha