Octane Engines | Cummins Inc.

Redefining the gasoline engine market

Octane offers the familiar, serviceable and user-friendly qualities found in gasoline engines, while also providing the performance of diesel at a low total cost of ownership thanks to longer maintenance intervals and improved fuel economy.

Benefits of gasoline

Gasoline possesses many benefits for both the vehicle and operator.

Widespread availability

The use of gasoline provides quick refueling times and increased fueling flexibility due to readily available refueling sites.

Driver familiarity

With low complexity air handling, no DEF required and no active regens, maintenance and operation are simplified.

Lower vehicle purchase price

Gasoline-powered vehicles typically cost less upfront and require less maintenance over the lifetime of the vehicle’s engine.

Established technology

Gasoline engine technology is well-developed and understood by mechanics globally.

b67 octane engine for vocational applications

Featured engine

B6.7 Octane

The Cummins B6.7 Octane engine is specifically designed and developed for the medium-duty market while achieving 2027 EPA and CARB compliance. Expanding the legacy of the Cummins B-series platform, the B6.7 Octane is equipped with the power, durability and performance of diesel with the simplicity of gasoline.

The capability to perform in demanding environments

B6.7 Octane has the power to work in challenging conditions such as hilly terrain and cold weather.

Hilly terrain with yellow sign

Hilly terrain

Steep inclines, rolling hills and winding roads are no obstacle for B6.7 Octane as it can maintain momentum without straining and allows for speed control.

Street during the winter season

Cold weather

The B6.7 Octane offers reliable starts in cold climates and performs well in cold temperatures as gasoline does not gel.

Alpha octane engine
Rocky Mount Engine Plant produces an alpha Octane engine

The first Alpha gasoline engine, B6.7 Octane, that the RMEP produced was built in the Value Package Introduction Lab.

Innovation. Technology and Services.

Cummins HELM™ Platforms

Cummins HELM™ Platforms

Cummins HELM™ is our industry's first series of engine platforms that allows customers to choose the fuel type that best suits their needs. The B series is a part of the innovation that continues to not only steer our company but also our industry in a brighter direction.

Connect with us