The Hanseatic on European Rivers | Cummins Inc.
""
Marine

The Hanseatic on European Rivers

by Alan Haig-Brown

Cummins Vessel Reference #568

The Hanseatic, Photo courtesy of Cummins Holland B.V.

The Hanseatic League was a highly successful trading alliance among northern European cities from the 13th to the 17th centuries. Some German cities continue to maintain an association under that name. Now the name Hanseatic is proudly emblazoned on the bow of a powerful inland-river boat built in the Netherlands for German owners.

The new MS Hanseatic I will be working the European rivers under the ownership of the Haak family. Like most of Europe’s inland vessels the accommodation in both the family quarters aft and the fo’c’sle are well equipped for creature comfort. To service the resulting electrical needs the vessel is fitted with a total of three Cummins 4BT3.9-G4-powered 45 kW generators sets. As is the practice on these rivers, larger capacity vessels are composed of the aft house powered cargo vessel with a second un-powered barge articulated forward of the first. This takes maximum allowance of the lock sizes. To manage this great length both the powered vessel and the barge are fitted with powerful bow thrusters. In this case the vessels each have thrusters powered by Cummins QSK15-C generating 410 kW (550 hp) each at 1800 RPM. These can be used to assist in directing the vessel into the locks as well as for stopping them once they are in the lock.

Used in conjunction with the vessel’s main engines the boat handler can be very precise in the positioning of the vessel. In the main engine room aft, the builders have installed twin Cummins QSK50-M mains engines each generating 1194 kW (1,600 hp) each at 1800 RPM. With a total installed propulsive power of 3208 kw (4362 hp) from all four engines this will be one of the most powerful vessels of her class on the European inland river system.

The MS Hanseatic I will also bear testament to the tenacious perseverance of the maritime trading ideals of the ancient Hanseatic League.


For more information, please contact:

Sjoerd Spronck
Advertisement & Promotion
Scandinavia and Benelux
Cummins Holland B.V.
Olivijn 800
3316 KH Dordrecht
The Netherlands
Tel: 31 78 6530 927
Fax: 31 78 6176 579
E-mail: [email protected]
Web: www.cummins.com | www.cummins.nl

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...