CO2 HDV Regulations: What do they mean for OEMs? | Cummins Inc.

CO2 HDV Regulations: What do they mean for OEMs?

By Cummins Europe, Global Power Technology Leader

Semis on highway

In May 2024, the European Council formally adopted an amendment to CO2 emission standards for heavy-duty vehicles (HDVs). This regulation applies stricter carbon emissions reduction targets to nearly all new heavy-duty vehicles, including commercial and vocational trucks, urban buses, and coaches. The goal is to achieve a 90% reduction in emissions by 2040.

How does the regulation affect vehicle OEMs? 

The bulk of the responsibility for meeting the CO2 emissions targets currently rests on vehicle OEMs, since carbon reductions will be measured on a fleet average basis using data from the VECTO tool. OEMs’ vehicle sales after 2025 will need to show the mandatory carbon reductions from their applicable baseline. This means that OEMs will need to sell an increasing number of vehicles powered by low- and zero-carbon technologies, mandating a change to traditional fossil-fuel based vehicle strategies.  

How will CO2 emissions be monitored? 

Crucial to monitoring CO2 emissions and fuel use is the Vehicle Energy Consumption Calculation Tool (VECTO). This data is mandatory for new trucks, buses and coaches above 3500 kg gross vehicle weight (GVW) and must be made publicly available. 

VECTO utilises engine, powertrain and vehicle data, with parameters such as rolling resistance, air drag, masses and inertias, to simulate CO2 emissions across HDVs. These results are then combined in different proportions depending on the vehicle’s sub-category. 

Compliance with EU CO2 reduction targets, assessed via VECTO, is based on CO2 emissions at the tailpipe as a result of fuel consumption. It doesn’t capture the small amounts of CO2 generated by AdBlue/DEF consumption or lubrication oils burning or what is produced through non-green hydrogen or electricity to charge batteries. There are also proposals to include the well to tank carbon intensity of the fuel, to give credit to biodiesel, HVO and e-fuels, but these developments are currently in their infancy. 

How have previous CO₂ regulations affected the on-highway market? 

Whenever new legislation is introduced, the industry adapts. Previous policy iterations has seen vehicle OEMs redesign cabs to make weight savings and provide room to incorporate new aftertreatment systems. Engines have also historically been downsped where required to support operation within lower emissions limits. 

We are now seeing power solutions providers innovating further to develop battery electric vehicles, hydrogen fuel cells and hydrogen combustion engines. The development of these technologies by Cummins means there are now multiple power options at an OEM’s disposal. Implementation of the stricter CO2 target is likely to accelerate uptake of these zero-carbon emissions technologies, assuming supporting fueling infrastructure can be delivered.  

Author Profiles

Cummins Europe, Global Power Technology Leader

Cummins Inc. opened its first site in Europe in 1956. Today it has 12 manufacturing sites and more than 10,800 employees in the region. Cummins works hard to provide advanced technologies supported by a long-established service network across Europe. Cummins is committed to investing in Europe through Research and Technology, ensuring Cummins’ technical experts are developing innovations of the future.

Want to find out more?

Receive the latest from Cummins in technologies, products, news, and insights.