Case Studies | Cummins Inc.

Cummins Case Studies

We’re in it for the long haul. We build lasting partnerships that lead to smarter innovations for our customers. These customer stories demonstrate our commitment and success in providing customers like you with improved power solutions through world-class innovation in a number of industries.

Filter Case Studies

As the shallowest part of the Bering Sea in Southwest Alaska, Bristol Bay is a treacherous region for vessels. Navigating strong winds amid the world’s highest tidal extremes with incredible shoals, sandbars and shallows is a required skill for commercial fishermen chasing the world’s largest salmon run. With all five Eastern Pacific species spawning in the bay's freshwater tributaries, includi

Cummins fuel cells equip world’s first commercial hydrogen fuel cell passenger ferry The only emission associated with Sea Change, the world’s first commercial hydrogen fuel cell passenger ferry, is pure (drinkable) water, produced from the fuel cells.  Built by All American Marine, the 21-meter, 75-passenger vessel is zero-emissions, hydrogen fuel-cell powered electric-drive ferry. Own

Cummins India powers world’s longest river cruise Even before its launch, M/V Ganga Vilas was destined for a rich legacy. With a sold-out manifest well into 2024, she is the first luxury cruise ship built in India. Additionally, this interesting passenger vessel was designed and built specifically to ensconce guests in the epitome of elegance and luxury for the world’s longest river cruise thro

Wherever the wind blows, Vagante wanders backed by Cummins While wandering means moving without planning, we’re certain a compass, navigational radar, and GPS guide S/Y Vagante to the most beautiful, remote, pristine places on the planet. After all, secluded islands, picturesque beaches, quaint coastal villages, and exciting passages are best explored by boat. Vagante is an incredible boat i

Magnolia One represents Turkish heritage and luxury Magnolia One is a diversion from the latest generation of yachts with exterior styling sometimes resembling white, plastic wedding cake stacks. Beckoning the golden age of yachting, Magnolia One’s graceful lines and fine craftsmanship radiate elegance, nostalgia, and Turkish charm. While dubbed a pocket superyacht, Magnolia’s DNA channels the

Following an intense storm and widespread power losses, Tulco Industrial Storage turned to Cummins to install seven generators and four transfer switches, as to keep the power on for its climate-controlled storage of mission-critical oilfield machinery.

The NEW Water wastewater treatment facility chose Cummins, after violent rainstorms left them without power for hours at a time, and two natural gas generator sets, and a DMC8000 Digital Master Control System was installed to ensure the facility continued to run smoothly through unpredictable weather conditions.

Imbued with natural light through large side hull windows, the spacious cabin of the Aquila 54 yacht power catamaran is elegant and comfortable, providing social spaces with panoramic 360° views. Offering three, four, and five cabin options as well as skipper’s quarters and galley-down layouts, this semi-custom production vessel meets an assortment of boating lifestyles. With a full-beam forwar

The newest passenger vessel for Fire Island Ferries, the “Fire Island Maid” is powered by Cummins QSL9's, with electrical power provided by a Onan MDK generator. The vessel operates primarily from Sayville to the fire island pines, taking passengers on an efficient and comfortable journey. The new Tier III compliant vehicle ferry designed by Elliott Bay Design Group is a 70-by-23-foot vessel i

The San Francisco Bay area is one of the world’s finest ports. Ships from around the world enter the Bay under the Golden Gate Bridge. Depending on their destination, they are likely to pass under at least one more of the Bay’s eight toll bridges. Not only do the bridges help both locals and visitors get to the other side of the Bay, but they also allow multiple ships to pass daily to piers throug

The Listuguj Mi’gmaq Government, an indigenous Canadian community on Quebec’s Gaspé Peninsula, has accepted delivery of a new 19.81 by 7.31-meter (65 x24-foot) combination crab trap and groundfish trawler. The vessel was designed by NAVANEX and built by Chantier Naval Forillon, both of Gaspé, Quebec, Canada. Named Ugjit Mijua’ji’jg in the Mi’gmaw language, the name means “For O

Repair, restoration and renovation of an old vessel is a significant undertaking. The reasons motivating a retrofit vary; however, in the case of Tivua, a 1982 Island Gypsy Europa MK1 retrofit, the impetus for change began in the engine room. “Before, the old engine oozed oil out of every corner,” said Rich Fricke, Tivua’s owner. “And we were so slow, running 7 - 7.5 knots and 6’s when windy. W

  Atlas, the famed Titan in Greek mythology, is renowned for bearing the world and sky on his shoulders, a punishment inflicted by Zeus on the strongest man in the world. Somewhere near St. Louis, MO, the mortal Atlas, a 65-foot triple screw towboat, is besieged with nearly the same fate in his working life on the Missouri and Mississippi Rivers. This inland river push boat is a comm

Levy Boats needed a reliable, powerful engine to get them through all seasons The colder the water, the better the fish. With no point more than 67 miles from the Atlantic Ocean, commercial fishermen face brutal elements with open sea in Nova Scotia. Fisheries for lobster, halibut and crab already have a limited season imposed by Mother Nature. Workboats employed for commercial fishing need

High-speed ferries need powerful engines day-in and day-out With high-transit networks converging on both sides, ferries built for high-speed travel must be well-built, stout and powerful. As a super volume commuter service for tourism operations, the vessel layout, speed, seakeeping ability and interior must be optimized for the mission. Such is the case of M/V Grey Lady IV, a 151-foot a

QSB6.7 propels interdiction vessel Somewhere, just over the horizon, an interdiction vessel is apprehending another criminal enterprise at sea. A great chase begins, frequently ending with Coast Guard Cowboys literally jumping from their rigid-hulled inflatable boat (RHIB) onto some partially submerged submarine, forcing open the hatch for takeover. Built to be fast, versatile and powerful i

Enforcing the law doesn’t just happen on land; it is also essential at sea. With record interdiction using tough, lightweight aluminum patrol boats, the success of the National Security Cutter program at apprehending criminals is remarkable. The 11M Long Range Interceptor II is just such a vessel, designed to pursue high-speed target craft for vessel board and seizure, rescue, and recovery. Eng

With the regulated catch quotas of contemporary fisheries, design versatility for a fishing boat can be important. A new 19.81 by 7.31-meter (65X24-foot) combination crab trap and groundfish trawler designed by NAVANEX for building by Chantier Naval Forillon, both of Gaspé, Quebec, Canada is a fine example of this. Owners, Listuguj Mi’gmaq Government, anticipate accepting delivery in April of 2022