Cummins CustomPaks | Cummins Inc.
custompaks ready for installation
Agriculture

Cummins CustomPaks

by Cummins Inc., Global Power Technology Leader

Cummins CustomPaks are being used for water management as Thailand struggles with its water crisis

Sixty Cummins CustomPaks are in service in Thailand as part of a critical water management plan aimed at easing the country’s water crisis – a crisis that has caused enormous economic and social damage and stirred conflict among communities.

Over the past several decades, Thailand has continually faced water problems caused by severe drought. Water reserves in dams and reservoirs are insufficient while water resources are often contaminated with toxins caused by urban communities and the industrial and agricultural sectors.

Severe flooding is a threat, too, at a time when the realities of climate change are hanging over the country. 

As a result, the allocation of precious water resources, which must be shared among various stakeholders including new and existing industry, large and small agriculture, and cities and villages has become a flashpoint.

Kittithanapat Engineering Co. (KTP), has been involved in the water management system since 1996, working closely with authorities such as the Royal Irrigation Department, Department of Water Resources, Bangkok Metropolitan Authority and others.

 

600 hp CustomPaks

To help KTP meet its often urgent requirements, Cummins DKSH (Thailand) has recently supplied 60 Australian-built CustomPaks – 45 powered by Cummins’ X15 engine rated at 600 hp, and 15 powered by the QSL9 rated at 325 hp. These fully self-contained powerpacks are emissions certified to Tier 3.

custompak engine

The CustomPaks are coupled to hydraulically-driven, large-volume submersible water pumps sourced by KTP from US company Moving Water Industries (MWI); KTP is the exclusive distributor in Thailand for these MWI Hydroflo pumps.

Prior to Cummins’ involvement, KTP was using another diesel engine brand but service support wasn’t up to the standard required.

Long-serving KTP engineer Kittisak Thanasoot says Cummins DKSH’s reputation for technical and aftersales support along with the reliability of the Cummins product were a key reason behind KTP’s decision to specify the CustomPaks for the Royal Irrigation Department. 

The ability of Cummins DKSH to respond to short delivery times was also important.

“Supplying large quantities of high horsepower diesel engines for emergency situations such as flash flooding can be a challenge for KTP,” says Kittisak Thanasoot.

“Responding to the needs of the government agencies to manage such problems in a timely manner and with least impact on communities, KTP has found the answer in our partnership with Cummins DKSH.”
 

Related case studies
Agriculture Case Study

White paper by Nicholas Hawes, CPE Technical Specialist Jump to: Introduction | Test Results | Summary   Executive Summary This paper provide...

Agriculture Case Study

Calling all farmers! We know that efficiencies help keep your business successful, so we’ve developed ten tips to help increase your fuel economy and save m...

Agriculture Case Study

In 2020, Kubota unveiled its largest tractor to date – the 19,510 lb. / 8550 kg M8. Its big features – power, reliability, comfort and value. Power comes...