Bleeder Brake | Cummins Inc.
Performance benefits of the Jacobs Bleeder Brake
  • Increases vehicle control
  • An ideal engine brake for smaller displacement engines
  • Reduces wear on the engine, tires, wheel-ends, and service brakes
  • Quiet operation for use wherever and whenever needed
  • Design flexibility to work with most engines
  • Low added weight
  • No camshaft required for engine braking
  • Use with a backpressure mechanism, such as an exhaust brake or variable geometry turbocharger (VGT), for maximum performance
 

How the Bleeder Brake works

When the bleeder brake is turned on, a piston extends to its full stroke and stays there, holding the exhaust valve open a small, fixed distance throughout the entire four-stroke engine cycle. Since the bleeder brake only holds the exhaust valve open a fixed distance, it is designed to not put any load on the camshaft and most of the overhead components.

  • The exhaust valve is held open throughout all four strokes of the engine cycle.
  • The compressed air “bleeds” out through the slightly opened exhaust valve during the entire compression stroke.
  • The engine pumps by pushing against the valve restriction and back pressure.
  • Bleeding off compressed air prevents the return of energy to the piston, which slows the vehicle down.
     

Bleeder Brakes can also be used in combination with a backpressure mechanism such as an exhaust brake or variable geometry turbocharger (VGT) for maximum braking performance.

Engine-specific solutions for leading OEMs

JVS partner — Deutz.

TCD 2013

JVS partner — DFM.

X7

JVS Partner — FAW.

6DL

JVS Partner — Ford Otosan.

Ecotorq 9

JVS partner — SDEC.

9L

JVS Partner — Volvo.

MDE8

JVS partner — Yuchai.

K10

Let's talk about your program

Our engineers are always available to discuss your current or future technology challenges. Contact us using this form, and a member of our team will contact you within two business days.

CAPTCHA