Many Islands, Many Ferries | Cummins Inc.
""
Marine

Many Islands, Many Ferries

by Alan Haig-Brown

Cummins Vessel Reference #648

Super Jet 19 at speed.

With over 230 million people living on about 13 thousand islands, Indonesia requires a lot of ferries. Shipyards such as PT. Bintan Marina Shipyard are meeting this demand for fast, safe and modern ferries. The yards recently designed, built and delivered the fast ferry, MV Super Jet 19, to the associated PT. Pelayaran Nasional Bahtera Bestari Shipping. The new boat continues a tradition of fine looking vessel designs that date back at least as far as the wooden Pinisi boats that continue their centuries old inter-island trade.


Sleek and fast.

While perhaps sharing some common ancestry, the MV Super Jet 19 is a vastly different vessel from the earlier inter-island traders. The sleek 34.7-meter by 5.5-meter ferry can transport up to 260 passengers at an average speed of 27 knots. The hull, with a 2.4-meter molded depth, holds tankage for 12,000 liters of fuel and 1,000 liters of water.

The hull also accommodates a powerful pair of Cummins KTA50-M2 engines each delivering 1600 HP at 1800 RPM to ZF Model BW455 gearboxes. Output from the gears is a pair of 110 mm by 5.5-meter long shafts with 1295 by 1016-m/m five-blade propellers. Electric power is provided by a pair of 60 kW generator sets.

With a crew of eight, the Super Jet 19 has capacity for up to 280 passengers. The new ferry is operating on a route between Tanjungpinang and Dabo Singkep in Indonesia.


Photos courtesy of Pt. Bintan Marina Shipyard

For more information:

Ms. Tresya
Director, Primarina Trading Pte. Ltd.
200 Jalan sultan, #15-06 Textile Centre
Singapore 199018
Phone: 65 9639 1050
E-mail: [email protected]

Selamat Budiman, BSc
PT. Pelayaran Nasional Bahtera Bestari Shipping
Jl.pos No.12/a – 14
Bintan Indah Mall Blok C Tj. Pinang
Indonesia 29111
Phone: 627 712 0000
Mobile: 62 812 706 8888
E-mail: [email protected]

Mr. Budiyanto
Branch Manager
PT Altrack 1978
Komplek Intl. Batam Business & Industrial Park,
Block A o. 3A
Sei Panas, Batam
Indonesia
Phone: 62 077 843 2412
Mobile: 62 812 7024 795
E-mail: [email protected]

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...