A Worker to Explore the Seabed | Cummins Inc.
""
Marine

A Worker to Explore the Seabed

by Alan Haig-Brown

Cummins Vessel Reference #564

Seabed Worker, Photo courtesy of Seabed AS/Cummins Norway AS

 

Mariners have become accustom to seeing ever more complex and sophisticated vessels launched in support of the petroleum exploration industry. A new level was set this year when the Norwegian yard Fjellstrand AS launched the multi-purpose offshore vessel Seabed Worker for Seabed AS of Begen Norway.

 

The DP2 classed vessel has two 2500 kW stern-mounted Voith propulsion units, a Rolls Royce 1000-kW tunnel bow thruster and a Rolls Royce 1000-kW retractable azimuthing bow thruster. Power for these electrically driven propulsion motors is provided by four Cummins QSK60 DMI-driven 1800 kW generator sets. The 88.8 by 16-meter vessel is packed with sophisticated equipment including two hydro-acoustic positioning reference systems and very broad suits of navigation and communications systems.

A ROV-hanger, situated aft of the accommodation area can be closed to provide a protected area for storage, maintenance and handling of the ROV. The 5.4 by 6-meter moon pool is fitted with a sliding hatch. Both the vessels two ROV launchers are fitted with active heave compensated winches with 4500 meters of umbilical capacity.

 

For more information:

 

Sjoerd Spronck
Advertisement & Promotion
Scandinavia and Benelux
Cummins Holland B.V.
Olivijn 800
3316 KH Dordrecht
The Netherlands
Tel: 31 78 6530 927
Fax: 31 78 6176 579
Web: cummins.com

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...