Yacht Class Working Boats | Cummins Inc.
""
Marine

Yacht Class Working Boats

by Alan Haig-Brown

Cummins Vessel Reference #823

A pair of the Colnago boats at speed.

 

Croatian tourism has grown by leaps and bounds in recent years. The great bulk of this is along the Adriatic coast where, as it has for centuries, life revolves around the sea. Tourists rent sail boats, take coastal cruises or travel to the many island that sit in the crystal Adriatic waters along the length of Croatia.

 

 

Luka Colnago in his shop at Split Croata. (Haig-Brown photo)

 

A popular way of experiencing the coast and its islands, is to hire a speed boat and have a knowledgeable local skipper take you out for a day trip. There are so many ways to spend the day with visits to places like the famous Blue Cave on Biševo Island or simply to anchor in a quiet bay for swimming and a picnic. This has created a demand for luxurious speed boats of 12 or 14 meters that regulations allow to carry up to 12 people plus two crew.

 

One of the leading firms producing this class of boat, is Colnago Marine in Split. Over the past ten years, explains owner Luka Colnago, “We have built 40 of these boats and we have several on order for 2018.”

 

 

On his roomy shop floor in early November there were three of the 14-meter models in varying states of construction while a fourth was being covered with a fairing compound, “These function as high end yachts to the people who charter them,” Colnago said, “So they require yacht quality finish both inside and out.”

 

 

On the Adriatic.

 

For day trips, speed is important. Colnago offers two propulsion packages. A single Cummins QSB 6.7 rated for 480 hp at 3000 RPM or two Cummins QSB 6.7 rated for 425 hp at 3000 RPM. In both configurations the engines turn propellers through ZF280 marine gears with 2:1 ratios. These propulsion packages result in cruising speeds, with a full load of passengers and crew, of 24 knots with the single engine and 34 knots with the twin engines.

 

 

A classy pair.

 

Speeds can vary to some extent given owners’ custom specifications as all design work is done in house. For example the dead-rise at the stern can be varied from as little as ten degrees for superior fuel economy to as much as 15 degrees for enhanced see-keeping values. Owners will make these decisions based on their operating locations and business preference. There are seven 12 and 14-meter boats on order this year to add to the 40 previous deliveries over the past ten years. All, but one, of these were for commercial day use with the one sold to a private customer for personal use.

 

The yard also builds nine to 12-meter RIBs for outboard power and has, in the past, delivered a pair of catamarans for support vessels at tuna farms.

 

Photo 1 Luka Colnago with one of his day boats under construction. (Haig-Brown)
Photos 2-6 Recently delivered high speed day tour boats by Colnago Marine. (Courtesy of Colnago Marine)

 

 

For further information:

 

Luka Colnago
President
Colnago Marine
Split Croatia
E-mail: [email protected]
Web: http://www.colnagomarine.com
Youtube: www.youtube.com/watch?v=H29ZUtyv0NY&feature=youtu.be

Goran Milavic
Assistant General Manager
Cummins Adriatic d.o.o.
Kraljice Jelene 15
21204 Dugopolje
Hrvatska (Croatia)
Phone: 385 0 21 668 647
Fax: 385 0 21 668 648
Mob: 385 0 91 124 4109
E-mail: [email protected]
Web: www.cummins.hr/reference/artmid/446/articleid/76/colnago-40

Related case studies
Marine Case Study

Trophy fish are measured by weight and length at the dock. They almost always exceed the size of the angler reeling them in. The exception would be M/V Chelsea ...

Marine Case Study

Greek passenger vessel repowers with Cummins.  Cruising to Symi on a water taxi is more than a boat ride across the Aegean Sea. Departing the eastern sh...

Marine Case Study

Crews with no choice but to head out to sea in rough weather conditions rely on trawlers' inherently robust, stout design based on the DNA of highly capable fis...